Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Controlling multiple WS2812B via UNO
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 417 subscribers
  • Views 1428 views
  • Users 0 members are here
  • frontpage
Related

Controlling multiple WS2812B via UNO

bassslapme
bassslapme over 9 years ago

So I have been asked to install a bunch of LED's into a friends fight stick as he knows nothing about them whilst I have a little experience with them. I have used WS2812B's as a backlight for my TV and used a HM-10 for it so i could make an app for it.

I wanted to reuse the app I made as it would mean cutting down the coding process, but I can't get my head around how I would control multiple sets of the strips. I would daisy chain each strip together via the DIN and DO, but when I put this in practice it just lights up the whole strip with whatever I set the first strip to. I believe maybe defining the individual strips would work ( # define LED_STRIP_A)

and then defining how many led are in that strips and applying the code for the different effects or just the RBG value for each pixel would work but I would like some pre-mental breakdown advice before I plunge into this and fail.

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 9 years ago +2
    Each LED in the strip is addressable. My understanding is that each WS2812 takes the data in, and subtracts one from the address and passes it out the Dout. For this example lets assume you have 4 lots…
Parents
  • mcb1
    mcb1 over 9 years ago

    Each LED in the strip is addressable.

    My understanding is that each WS2812 takes the data in, and subtracts one from the address and passes it out the Dout.

     

    For this example lets assume you have 4 lots of 10 LED's. You can address all 40 and use a loop to assign the RGB setting to 0-39

    OR you could have 4 seperate loops of 0-9, 10-19, 20-29, 30-39 and set the colour for each of the LED's and step through the 10 times to give the effect.

     

    You can send all the settings and then execute the strip.show which makes them display the revised setting.

    So in essence the LED's are doing the data array for you.

     

    If you are worried about persistance of vision, then the DotStar use a data and clock and can run much higher data rates.

    https://www.adafruit.com/product/2343

    https://www.adafruit.com/product/2237

     

    Hope this helps.

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 9 years ago

    Each LED in the strip is addressable.

    My understanding is that each WS2812 takes the data in, and subtracts one from the address and passes it out the Dout.

     

    For this example lets assume you have 4 lots of 10 LED's. You can address all 40 and use a loop to assign the RGB setting to 0-39

    OR you could have 4 seperate loops of 0-9, 10-19, 20-29, 30-39 and set the colour for each of the LED's and step through the 10 times to give the effect.

     

    You can send all the settings and then execute the strip.show which makes them display the revised setting.

    So in essence the LED's are doing the data array for you.

     

    If you are worried about persistance of vision, then the DotStar use a data and clock and can run much higher data rates.

    https://www.adafruit.com/product/2343

    https://www.adafruit.com/product/2237

     

    Hope this helps.

    Mark