Arduino
  • Products
  • More
Arduino
Arduino Forum LoRa transceiver
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 416 subscribers
  • Views 1496 views
  • Users 0 members are here
Related

LoRa transceiver

tim2
tim2 over 8 years ago

i would like to use LoRa SX1278 and Arduino for detection of garage remote control key and other 433 MHz sensors at home.  can anyone advise me?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +1
    Hi Kutil, You won't get long-range reception of garage key and other sensors. That's because they don't use LoRa, so your LoRa receiver chip will be operating in normal FSK reception mode. In which case…
  • tim2
    tim2 over 8 years ago in reply to shabaz +1
    Thanks, and what about short range reception ( 100 m ) ? In parameters I found parameter - mode - LORA, I think when I'll somehow change it, I'll receive a signal for short distance. My goal is identify…
  • shabaz
    shabaz over 8 years ago in reply to tim2 +1
    Hi Kutil, Could you clarify what you mean by identify and not decode? There may be other (easier) ways to achieve what you need, but I just want to be sure of your requirement. You just want to see the…
Parents
  • BigG
    BigG over 8 years ago

    If you have +$100 to splash out then maybe this RF spectrum analyser would do the trick Official RF Explorer home to at least give an indication which channels are being used.

     

    In my experience, I found that the SI4463 transceiver chip offered a better range than cc1101. I had two HC-12 433MHz wireless module (based on this chip) "talking" to each +100m apart.

     

    Depending on how many channels are being broadcast on you could simply hook up a couple (where each one configured to listen on a different channel) to a good microcontroller which has multiple serial ports etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • BigG
    BigG over 8 years ago

    If you have +$100 to splash out then maybe this RF spectrum analyser would do the trick Official RF Explorer home to at least give an indication which channels are being used.

     

    In my experience, I found that the SI4463 transceiver chip offered a better range than cc1101. I had two HC-12 433MHz wireless module (based on this chip) "talking" to each +100m apart.

     

    Depending on how many channels are being broadcast on you could simply hook up a couple (where each one configured to listen on a different channel) to a good microcontroller which has multiple serial ports etc.