Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Sauna Heater Control. Help Needed.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 417 subscribers
  • Views 5101 views
  • Users 0 members are here
Related

Sauna Heater Control. Help Needed.

studioab
studioab over 8 years ago

I've finished my first IoT project based on Arduino Yun. It's a remote control for my sauna. Everything is working as expected in test mode (relay is not connected to contactor so there is no real load), I was able to test this system for hours without any problems.

 

When I hook up contactor to relay, it turns the heater on and off, and everything seems to be working, but after a while (absolutely random, it could be an hour or a few minutes) LCD screen freezes, or sometimes, starts flashing random symbols, server is not responding to commands, rotary encoder isn't working and it seems Arduino freezes. The only workaround is to turn off the power and reset the system. After it restarts, everything is back to normal.

 

I came across this post 16*2 LCD getting weird characters symptoms are the same, I think high AC load is causing EMF impulse that is crashing Arduino. Power Module, Relay board, LCD, and Arduino board are really close to each other and inside the box.

 

I'm not sure if it violates the rules, but I would like to mention these people from the other post @WarrenW @Robert Peter Oakes @Gough Lui @neilk @D_Hersey

 

I think here are my options. What would you recommend to do?

 

- replace relays with solid state relay

- shield AC wires

- remove power module from the box

- don't use the same power module for relays

- ???

Attachments:
image
image
image
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago in reply to studioab +4
    I would like to say huge thank you to all people that contributed to this thread. I was able to eliminate all the issues causing arduino to crash Glad we could help. Do you guys think this project should…
  • jw0752
    jw0752 over 8 years ago +3
    Hi Eugene, The answer might be as simple as adding more decoupling capacitance with low ESR to the power feed to the Arduino. This can be done by putting a 100 nF capacitor and a 100 uF cap in parallel…
  • ralphjy
    ralphjy over 8 years ago +3
    Hi Eugene, Nice looking project. I would suspect your problem is that the 240V input glitches when your load switches and that causes the 5V to glitch. If you had a scope you could monitor the 5V supply…
Parents
  • ralphjy
    ralphjy over 8 years ago

    Hi Eugene,

     

    Nice looking project.  I would suspect your problem is that the 240V input glitches when your load switches and that causes the 5V to glitch.  If you had a scope you could monitor the 5V supply.

     

    I guess it is not convenient to isolate the 5V supply from the 240V (e.g. if you had a separate 120V circuit), but that probably would fix it.  Replacing the relay with a solid state relay probably won't help unless your circuit load is close to the 2A capacity of the 5V supply (have you measured the supply current with the relay on?).  If it is very intermittent maybe an additional filter capacitor on the 5V output would help.

     

    Ralph

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ralphjy
    ralphjy over 8 years ago

    Hi Eugene,

     

    Nice looking project.  I would suspect your problem is that the 240V input glitches when your load switches and that causes the 5V to glitch.  If you had a scope you could monitor the 5V supply.

     

    I guess it is not convenient to isolate the 5V supply from the 240V (e.g. if you had a separate 120V circuit), but that probably would fix it.  Replacing the relay with a solid state relay probably won't help unless your circuit load is close to the 2A capacity of the 5V supply (have you measured the supply current with the relay on?).  If it is very intermittent maybe an additional filter capacitor on the 5V output would help.

     

    Ralph

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • studioab
    studioab over 8 years ago in reply to ralphjy

    Thank you for all your suggestions. I want to assure you that all wires from the master switch to the sauna box and to the heater, contactor, 65A breakers, fuses are installed according to specs by professional electrician. Sauna heater is working fine with the old control module that came with it.

     

    Contactor that came with the heater is rated 40amp per terminal, and as far as I understand, 37.5A is actually 18.7A per leg (120 L1/L2) so it should be enough.

     

    • I checked the voltage with the electronic voltmeter between L1/L2 (240) line during start/stop, no drops or spikes, 5V output is also stable (issues reproes only after heater starts working, sometimes even after 1 hour or so)
    • This is the relay board that I’m using right now, I think Arduino is fully capable of running it.
    • I was testing the whole system for multiple hours without heater, everything is working as expected

     

    This is what I will try to do next, please let me know what you think:

     

    1. Remove the heater wires from contactor and test the system with contactors coli only
    2. Replace relays with solid state relays, it's rated 2A output and it should be more than enough to power contactor’s coil
    3. Shield and filter all DC wires coming to Arduino from LCD and Encoder
    4. If #2 doesn’t help, I will try to use batteries to power the system and if it helps I will remove high voltage components (power module and relay) from the box and keep them away from Arduino and LCD

     

    I could be wrong with my assumption here, but I noticed that almost all the time Arduino crashes right after contactor turns off the heater. I haven't seen any issues when contactor turns on the heater.