Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Cant receive data from arduino via bluetooth
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 416 subscribers
  • Views 1787 views
  • Users 0 members are here
Related

Cant receive data from arduino via bluetooth

happyforever
happyforever over 8 years ago

I can receive data from android but cant send data to android, please help me to solve. The below is my code.

Board I used is arduino uno and external module is HC-06.


#include <SoftwareSerial.h>

 

int bluetoothTx = 13;  // TX-O pin of bluetooth mate, Arduino D2

int bluetoothRx = 14;  // RX-I pin of bluetooth mate, Arduino D3

 

char incomingByte; // incoming data

int sensorPin = A0;  

int ledPin = 11;      // select the pin for the LED

int ledPin2 = 12;

int sensorValue = 0;  // variable to store the value coming from the sensor

int rTrigPin = 6;

int rEchoPin = 7;

int trigPin = 9;

int echoPin = 10;

int lTrigPin = 4;

int lEchoPin = 5;

 

// defines variables

long rDuration;

int rDistance;

long duration;

int distance;

long lDuration;

int lDistance;

 

 

SoftwareSerial bluetooth(bluetoothTx, bluetoothRx);

 

void setup() {

 

  Serial.begin(115200);

 

  bluetooth.begin(115200);  // The Bluetooth Mate defaults to 115200bps

  //bluetooth.print("$");  // Print three times individually

  //bluetooth.print("$");

  //bluetooth.print("$");  // Enter command mode

  //delay(100);  // Short delay, wait for the Mate to send back CMD

  //bluetooth.println("U,9600,N");  // Temporarily Change the baudrate to 9600, no parity

  // 115200 can be too fast at times for NewSoftSerial to relay the data reliably

  bluetooth.begin(9600);  // Start bluetooth serial at 9600

 

  pinMode(rTrigPin, OUTPUT); // Sets the rTrigPin as an Output

  pinMode(rEchoPin, INPUT); // Sets the rEchoPin as an Input

  pinMode(trigPin, OUTPUT); // Sets the trigPin as an Output

  pinMode(echoPin, INPUT); // Sets the echoPin as an Input

  pinMode(lTrigPin, OUTPUT); // Sets the lTrigPin as an Output

  pinMode(lEchoPin, INPUT); // Sets the lEchoPin as an Input

 

 

  // declare the ledPin as an OUTPUT:

  pinMode(ledPin, OUTPUT);

  pinMode(ledPin2, OUTPUT);

}

 

/*void loop() {

  // read the value from the sensor:

  sensorValue = analogRead(sensorPin);

  // turn the ledPin on

  digitalWrite(ledPin, LOW);

  // stop the program for <sensorValue> milliseconds:

  delay(sensorValue);

  // turn the ledPin off:

  digitalWrite(ledPin, HIGH);

  // stop the program for for <sensorValue> milliseconds:

  delay(sensorValue);

  }*/

 

void loop()

{  

        digitalWrite(rTrigPin, LOW);

        delayMicroseconds(2);

        digitalWrite(rTrigPin, HIGH);

        delayMicroseconds(10);

        digitalWrite(rTrigPin, LOW);

        rDuration = pulseIn(rEchoPin, HIGH);

        rDistance = (rDuration / 2) / 29.1;

    

        digitalWrite(trigPin, LOW);

        delayMicroseconds(2);

        digitalWrite(trigPin, HIGH);

        delayMicroseconds(10);

        digitalWrite(trigPin, LOW);

        duration = pulseIn(echoPin, HIGH);

        distance = (duration / 2) / 29.1;

    

        digitalWrite(lTrigPin, LOW);

        delayMicroseconds(2);

        digitalWrite(lTrigPin, HIGH);

        delayMicroseconds(10);

        digitalWrite(lTrigPin, LOW);

        lDuration = pulseIn(lEchoPin, HIGH);

        lDistance = (lDuration / 2) / 29.1;

    

        sensorValue = analogRead(sensorPin);

 

 

          if (rDistance <= 221 || distance <= 221 || lDistance <= 221)

        {

          if (sensorValue <= 140)

          {

            digitalWrite(ledPin, LOW);

            digitalWrite(ledPin2, LOW);

          }

          else

          {

            digitalWrite(ledPin, HIGH);

            digitalWrite(ledPin2, HIGH);

          }

          

        }

        else if (rDistance > 221 || distance > 221 || lDistance > 221)

        {

          if (sensorValue <= 140)

          {

            digitalWrite(ledPin, LOW);

            digitalWrite(ledPin2, LOW);

          }

          else

          {

            digitalWrite(ledPin, HIGH);

            digitalWrite(ledPin2, HIGH);

          }

        }

 

  if (bluetooth.available()) // If the bluetooth sent any characters

  {

    // Send any characters the bluetooth prints to the serial monitor

  

    Serial.println((char)bluetooth.read());

    incomingByte = bluetooth.read();

 

 

  

    if(incomingByte == '1') {

 

 

         Serial.println("Music is pause and now you are in dangerous situation.");  // print message

         //bluetooth.print("1");

       

         //delay(1000);

    }

 

    if(incomingByte == '0') {

    

          digitalWrite(ledPin, HIGH);

          digitalWrite(ledPin2, HIGH);

          Serial.println("Alert signal OFF and music would not pause when in dangerous situation.");  // print message

          //bluetooth.print("0");

          //delay(1000);

          //break;

        

    }

  }

 

 

  if (Serial.available()>0) // If stuff was typed in the serial monitor

  {

    int bytes=Serial.available();

    //Serial.readBytes(buffer, startPosition, bytes);

 

    bluetooth.print((char)Serial.read());

  

  }

 

}



  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 8 years ago +2
    Hello happyforever I have replied to your other post here: Sending serial data from Arduino to Android via Bluetooth - NOT ANSWERED Yet
  • neilk
    neilk over 8 years ago +2
    Hi happyforever It's often a good idea to test out various components of a program separately and when they all work, combine them together slowly, making sure each addition still works. Your question…
  • neilk
    neilk over 8 years ago in reply to gadget.iom +1
    Hi gadget.iom - sorry Neil
Parents
  • neilk
    neilk over 8 years ago

    Hi happyforever

     

    It's often a good idea to test out various components of a program separately and when they all work, combine them together slowly, making sure each addition still works.

     

    Your question relates to the Bluetooth communication from Arduino to Android, via HC06 BT adapter. If I were you. I would use a very simple program to prove that communication works, before developing the program further.

     

    Note that the HC06 device normally comes configured for 9600  - not sure what your use of 115,200 relates to, but I see you abandon that and as mcb1 has said, most, if not all your output to the Bluetooth device is commented out, so not much is likely to happen.

     

    My blog, where you also pose this same question, shows a very simple example of sending data from an Arduino via Bluetooth, which you should be able to get working.

     

     

    Sometimes it's hard to see the wood for the trees.

     

    Neil

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 8 years ago in reply to neilk

    Hi neilk

    I think you might be confusing me with mcb1. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 8 years ago in reply to gadget.iom

    Hi gadget.iom - sorry

     

    Neil

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • happyforever
    happyforever over 8 years ago in reply to neilk

    Hi Neil can you help me see my android code? I think my error come from android code there. Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 8 years ago in reply to happyforever

    Sorry - I develop my Android Apps at a much higher level, using MIT AppInventor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • neilk
    neilk over 8 years ago in reply to happyforever

    Sorry - I develop my Android Apps at a much higher level, using MIT AppInventor.