Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Noobie with newb questions for simple project
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 415 subscribers
  • Views 1399 views
  • Users 0 members are here
Related

Noobie with newb questions for simple project

masterbri
masterbri over 8 years ago

Hiw are y’all doin!! So, I’ve been playing around with an arduino project for quite a while now and finally got it to work after a year of tinkering. I was working on what seemed like a fairly straight forward led matrix thing using glediator and an Arduino UNO.

 

My current project that I’ve been looking into seems a little more complex to me in that I want to actually have different systems communicating with each other. I’m sure this is kinda child’s play to yall out there that are more familiar with this stuff so please bear with me as I still consider myself quite illiterate in this field!

 

heres my situation: I have two separate objects, one is essentially a transporter and the other would be package. The transporters job is to lift the package and move it to another location. I plan to have an Arduino UNO with an rfid sheild mounted in the transporter and an rfid tag mounted on the package. The first goal is to have the transporter read that the package is near and activate a switch that drops the lifting mech.

The transporter is also outfitted with a photo sensor that triggers an audible alarm letting me know when the package is centered on the lifting mech. The second goal is the have the arduino recognize that the sensor has been triggered, say for 3 seconds, and then activate he other switch which would raise the lifting mech.

 

To me it it seems like two gairly straightforward operations. my biggest obstacle is figuring out how to write a code to handle these two distinct operations within the ide, from scratch

 

i sure appreciate any help y’all could provide!!

thanks, Brian

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +4
    Hi Brian, I'm not sure it is as straightforward as you suggest : ( The devil is in the detail. At a high level, the pseudocode is simple: while(1) { result=readTag(); if(result) { lifting_mechanism…
  • beacon_dave
    beacon_dave over 8 years ago +3
    Perhaps take a look at this RFID tutorial: Tutorial 12 for Arduino: RFID Card Reading It's for a door lock however it covers a lot of the elements your project requires, namely the reading of a RFID tag…
  • fmilburn
    fmilburn over 8 years ago in reply to masterbri +2
    Updated suggestion for mains relay in USA: https://www.adafruit.com/product/2935
Parents
  • shabaz
    shabaz over 8 years ago

    Hi Brian,

     

    I'm not sure it is as straightforward as you suggest : ( The devil is in the detail. At a high level,  the pseudocode is simple:

    while(1)
    {
      result=readTag();
      if(result)
      {
         lifting_mechanism=1;
      }
      if (photosensor==1)
      {
         alarm=1;
      }
      else
      {
        alarm=0;
      }
    }

     

    In practice, you'd need to decide when to set the lifting mechanism output back to zero, and find a way of getting a reliable photosensor output in all lighting conditions, and decide how often you wish to scan the imputs and use a sleep or wait type of instruction. In any case, the pseudocode meets the requirement as you stated, I'm just suggesting that the system will be more complicated than that. There are also better ways to code the solution, but is a bit more complicated - if you explore the topic of 'interrupts' you'll see some ways to modify the code so that it doesn't need to scan/poll inputs.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 8 years ago

    Hi Brian,

     

    I'm not sure it is as straightforward as you suggest : ( The devil is in the detail. At a high level,  the pseudocode is simple:

    while(1)
    {
      result=readTag();
      if(result)
      {
         lifting_mechanism=1;
      }
      if (photosensor==1)
      {
         alarm=1;
      }
      else
      {
        alarm=0;
      }
    }

     

    In practice, you'd need to decide when to set the lifting mechanism output back to zero, and find a way of getting a reliable photosensor output in all lighting conditions, and decide how often you wish to scan the imputs and use a sleep or wait type of instruction. In any case, the pseudocode meets the requirement as you stated, I'm just suggesting that the system will be more complicated than that. There are also better ways to code the solution, but is a bit more complicated - if you explore the topic of 'interrupts' you'll see some ways to modify the code so that it doesn't need to scan/poll inputs.

    • Cancel
    • Vote Up +4 Vote Down