Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Coding trouble
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 416 subscribers
  • Views 2553 views
  • Users 0 members are here
Related

Coding trouble

tech_nut81
tech_nut81 over 8 years ago

Hi all. I was wondering if anyone more experienced than myself would be willing to take a look at this code and help me understand what's going wrong. I keep getting this error message, "error: unterminated argument list invoking macro "F".

 

I'll fill ya in on what I'm trying to do. I want to control the water level in a tank using a float switch, solenoid valve and the arduino. I was using just the float switch and solenoid valve connected through a relay, but whenever the water level would start dropping due to water usage, the solenoid would cycle on and off very quickly while keeping the water level up. What I want to do is have the arduino put in a 2 minute delay when the switch is activated so that the tank fills up smoothly.

 

Comments, suggestions and ideas are all appreciated.

 

DJ

Attachments:
Solenoid control.zip
  • Sign in to reply
  • Cancel

Top Replies

  • tech_nut81
    tech_nut81 over 8 years ago in reply to andywest +4
    You're right andywest , it was the double quote. I went back in a put all the F macros back in and only removed the double quotes. Compiling completed successfully after that. Thank you so much for taking…
  • andywest
    andywest over 8 years ago +3
    The F() macro is defined in WString.h , which is part of the core Arduino package. If I understand correctly, it stores a string constant in flash rather than RAM. Very useful in situations where RAM is…
  • tech_nut81
    tech_nut81 over 8 years ago in reply to shabaz +3
    Awesome! I removed all instances of 'F( and the subsequent extra ')' . After that there were a few more errors regarding extra quotation marks. Once I removed all of those compiling was successful. The…
Parents
  • shabaz
    shabaz over 8 years ago

    Hi,

     

    You've got something odd on many lines in Firmware.ino -

    for example on line 73, it says:

    Serial.println(F("\nWhich component would you like to test?"));

     

    Wherever you got the code from, someone may have created some macro 'F' (bad name for a macro) for some reason or other (no idea). In any case, if the macro no longer exists, then these Serial.println lines (there are many of them like this) need to change.

    You could strip off the characters 'F('  and one of the closing brackets, so that line 73 becomes:

    Serial.println("\nWhich component would you like to test?");

     

    That should get it to compile (or at least move on to any next error).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 8 years ago

    Hi,

     

    You've got something odd on many lines in Firmware.ino -

    for example on line 73, it says:

    Serial.println(F("\nWhich component would you like to test?"));

     

    Wherever you got the code from, someone may have created some macro 'F' (bad name for a macro) for some reason or other (no idea). In any case, if the macro no longer exists, then these Serial.println lines (there are many of them like this) need to change.

    You could strip off the characters 'F('  and one of the closing brackets, so that line 73 becomes:

    Serial.println("\nWhich component would you like to test?");

     

    That should get it to compile (or at least move on to any next error).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • tech_nut81
    tech_nut81 over 8 years ago in reply to shabaz

    Awesome! I removed all instances of 'F( and the subsequent extra ')' . After that there were a few more errors regarding extra quotation marks. Once I removed all of those compiling was successful.

     

    The project continues....

     

    Thank you shabaz

    • Cancel
    • Vote Up +3 Vote Down