Arduino Forum Importing data from MCU to MATlab
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
  • Replies 3 replies
  • Subscribers 391 subscribers
  • Views 600 views
  • Users 0 members are here
  • gizduino
  • fire
  • matlab
  • mcu
  • arduino
Related

Importing data from MCU to MATlab

Former Member
Former Member over 9 years ago

Hi! We have this project for our senior's research regarding the optimization of multiple sensors which incorporates DS Theory. I would like to know if any of you knows how to import data from a microcontroller into MATlab program?:-D

  • Sign in to reply
  • Cancel
  • michaelkellett
    michaelkellett over 9 years ago

    The simplest way is to use a serial interface - buy a USB to serial dongle for the PC, then use the built in support for serial ports in MATLAB to talk to the micro via one of its built in UARTS. If you buy an FTDI USB<->serial lead with logic level UART interface you can connect this directly to the UART ports on the micro.

     

    If you need more bandwidth then use a  micro with built in Ethernet and the built in support for network comms in the very latest release of MATLAB - this is more work (since you'll almost certainly need a lot more code and extra chips at the micro end) but can go faster and has other advantages.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago

    MATLAB has a direct interface for the most commonly used boards (Uno, Mega, Due, Leonardo) at Arduino Support from MATLAB - Hardware Support

     

    This is much easier than trying to do your own bit-banging.  The interface  is just an ordinary USB cable from the PC to port on the Arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to Former Member

    There is a MATLAB package that you use to abstract the serial connection to both transmit instructions to, and receive data from the Arduino.  The link I included in my post gives you "how-to" videos, code examples, and a documentation package.  Only caveat is you need to have MATLAB R2014a or higher.  There is more than one way to do it, but; for instance say I wanted to connect to an Arduino Uno on the USB port COM4, and use a TMP102 I2C temp sensor.

     

    1.     Start the connection:  a = arduino ( 'com4', 'uno', 'Libraries', 'I2C')

    2.     Scan the I2C bus: addrs = scanI2CBus(a)

    3.     We'll say the only I2C address this returns is 0x298

    4.     You create the I2C object: tmp102 = i2cdev(a, '0x298')

    5.     And write the code to retrieve the Celsius temp using I2C:

                   write(tmp102, 0, 'uint8');

                     data = read(tmp102, 2, 'uint8');

                    temperature = (double(bitshift(int16(data(1)), 4)) + double(bitshift(int16(data(2)), -4))) * 0.0625

     

     

    This is a screenshot of a demo on the MathWorks website using MATLAB R2015a.  They've tried to make the API's close to Arduino syntax.