Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Measuring speed, angle and height
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 420 subscribers
  • Views 5077 views
  • Users 0 members are here
  • object
  • flying
  • angle
  • arduino
  • speed
  • height
Related

Measuring speed, angle and height

SGarciaV
SGarciaV over 11 years ago

Hi all,

 

I am discussing a possible project, but I am not certain how feasible it is. The project consists of using an Arduino, plus some sensor (or sensors) to measure the speed, angle and height of a flying object over a 6 x 30 cm surface. Although I am unfamiliar with the details, the object will pass over the surface and the Arduino needs to get how fast it is moving, the angle at which it crosses the surface and the distance from the surface to the object.

 

I posted a rough sketch below.

 

Can some one please provide some feedback as to how feasible this is and what sort of sensor(s) will be needed? Thanks! Salvador

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +1
    Here is a technique that might work - the accuracy depends on how well it is implemented. start with a narrow beam LED (preferably collimated) or a laser shine it through a section of a cylindrical lens…
  • SGarciaV
    SGarciaV over 10 years ago in reply to bhavikbhansali +1
    Hi Bhavik! Thank you for your reply. The object is a tennis ball traveling at approximately 70 to 90 miles per hour. Salvador
Parents
  • peterjcs23
    peterjcs23 over 11 years ago

    TI make a pretty good ultrasound chip you might consider.

     

    http://www.ti.com/lit/ds/symlink/pga450-q1.pdf

     

    and this might help too.

     

    http://e2e.ti.com/blogs_/b/analogwire/archive/2015/07/31/time-of-flight-measurements-using-high-performance-time-to-digital-converters

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • peterjcs23
    peterjcs23 over 11 years ago

    TI make a pretty good ultrasound chip you might consider.

     

    http://www.ti.com/lit/ds/symlink/pga450-q1.pdf

     

    and this might help too.

     

    http://e2e.ti.com/blogs_/b/analogwire/archive/2015/07/31/time-of-flight-measurements-using-high-performance-time-to-digital-converters

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • SGarciaV
    SGarciaV over 11 years ago in reply to peterjcs23

    Thanks Peter, I will have a look at the links that you posted. Salvador

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to peterjcs23

    Salvador can't use a classical ultrasonic distance measuring system because the tennis ball moves much too fast - he has a total window of about 1.5ms as it goes past and he needs to measure it's position at least 3 times in that window. So at 0.5mS per measurement there isn't time to send a pulse and wait for an echo. (If the ball is 30cm away it's  a 2ms round trip time.)

     

    Hence my suggestion of ultrasound illumination with a modulated carrier - but it won't be easy to demodulate the echoes because the Doppler shift will affect the return signal making it harder to lock onto the modulation (which you have to do to estimate the time from the transmitter to the tennis ball.)

     

    (It's a fun project but I wouldn't look at it commercially for less than £50k for a working prototype !)

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • peterjcs23
    peterjcs23 over 11 years ago in reply to michaelkellett

    It all sounds like a bit of a stretch for an arduino in real time. You could use an array of ultrasound receivers and measure time delays. The ball will be long gone by the time you've done the calculations. You stand a pretty good chance of missing the  ball altogether.

     

    Or perhaps an array of light sensors detecting a laser scan rather than a full image scheme. It would have to be in 2 orthogonal planes.