Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Measuring speed, angle and height
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 420 subscribers
  • Views 5090 views
  • Users 0 members are here
  • object
  • flying
  • angle
  • arduino
  • speed
  • height
Related

Measuring speed, angle and height

SGarciaV
SGarciaV over 11 years ago

Hi all,

 

I am discussing a possible project, but I am not certain how feasible it is. The project consists of using an Arduino, plus some sensor (or sensors) to measure the speed, angle and height of a flying object over a 6 x 30 cm surface. Although I am unfamiliar with the details, the object will pass over the surface and the Arduino needs to get how fast it is moving, the angle at which it crosses the surface and the distance from the surface to the object.

 

I posted a rough sketch below.

 

Can some one please provide some feedback as to how feasible this is and what sort of sensor(s) will be needed? Thanks! Salvador

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +1
    Here is a technique that might work - the accuracy depends on how well it is implemented. start with a narrow beam LED (preferably collimated) or a laser shine it through a section of a cylindrical lens…
  • SGarciaV
    SGarciaV over 10 years ago in reply to bhavikbhansali +1
    Hi Bhavik! Thank you for your reply. The object is a tennis ball traveling at approximately 70 to 90 miles per hour. Salvador
Parents
  • dougw
    dougw over 10 years ago

    Here is a technique that might work - the accuracy depends on how well it is implemented.

    • start with a narrow beam LED (preferably collimated) or a laser
    • shine it through a section of a cylindrical lens to create a light beam that looks like a vertical line or "plane" of light
    • oscillate the light at some frequency above 100 KHz - the higher the frequency the more accurate the speed measurement can be
    • use a light sensor to detect reflections of the light off the ball as it goes through the beam
    • a high-pass filter or bandpass filter on the sensor signal will eliminate ambient light
    • count the number of reflected pulses to know how long the ball was in the beam - this is a measure of ball speed
    • use the same type of system except make the light plane horizontal instead of vertical, and again count pulses as the ball passes through the second beam
    • knowing the speed from the first beam, you can calculate the angle of trajectory by how long it takes to pass through the second beam

    Of course it only works if the ball passes all the way through both beams. If the second beam is not horizontal, say it is at 45 degrees, it is still possible to calculate trajectory angle, but it is harder to get an accurate measurement.

    With a PSoC4 you could make a rudimentary system for under $10 in parts, ($15 if you include a display)

    An arduino should also be fast enough to count these pulses.

    You could do even this without even needing a microcontroller - just some counters and logic.

    Doug

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • SGarciaV
    SGarciaV over 10 years ago in reply to dougw

    Thanks Douglas.I had mentioned to him about using lasers, but my idea consisted of using multiple lasers to create the plane, instead of one laser passing through a cylindrical lens to create the plane. I am intrigued enough by your idea that if I can make the time I might test it out myself.Thanks for your input! Salvador

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • SGarciaV
    SGarciaV over 10 years ago in reply to dougw

    Thanks Douglas.I had mentioned to him about using lasers, but my idea consisted of using multiple lasers to create the plane, instead of one laser passing through a cylindrical lens to create the plane. I am intrigued enough by your idea that if I can make the time I might test it out myself.Thanks for your input! Salvador