Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Measuring speed, angle and height
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 420 subscribers
  • Views 5107 views
  • Users 0 members are here
  • object
  • flying
  • angle
  • arduino
  • speed
  • height
Related

Measuring speed, angle and height

SGarciaV
SGarciaV over 11 years ago

Hi all,

 

I am discussing a possible project, but I am not certain how feasible it is. The project consists of using an Arduino, plus some sensor (or sensors) to measure the speed, angle and height of a flying object over a 6 x 30 cm surface. Although I am unfamiliar with the details, the object will pass over the surface and the Arduino needs to get how fast it is moving, the angle at which it crosses the surface and the distance from the surface to the object.

 

I posted a rough sketch below.

 

Can some one please provide some feedback as to how feasible this is and what sort of sensor(s) will be needed? Thanks! Salvador

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +1
    Here is a technique that might work - the accuracy depends on how well it is implemented. start with a narrow beam LED (preferably collimated) or a laser shine it through a section of a cylindrical lens…
  • SGarciaV
    SGarciaV over 10 years ago in reply to bhavikbhansali +1
    Hi Bhavik! Thank you for your reply. The object is a tennis ball traveling at approximately 70 to 90 miles per hour. Salvador
Parents
  • jc2048
    jc2048 over 10 years ago

    Rather than use a camera with it's very limited frame rate, you could use several linear sensor arrays like these:

     

    http://www.digikey.co.uk/product-detail/en/TSL1401CL/TSL1401CLCT-ND/3095283

     

    If you placed a wide angle lens, with a 90 degree field of view, in front of the device you'd have a fan-like view. One at each of the front corners, facing towards each other and up would give you the ability to do triangulation on a plane rising from the front. With another pair at the back, you'd then have enough information to do the timing and the trajectory. Wouldn't work for small objects, but might be ok for your tennis ball.

     

    They'd be much faster than a camera. You'd need a decent a/d. Haven't looked at sensitivity (adaption to varying light levels) and would have problems with background motion (people moving around) if it wasn't screened. Whether you could do all the processing with an Arduino I don't know - I would think not.

     

    Might not be necessary to digitise; if there were enough contrast between the ball and the background (enhance with a filter?) you could use a comparator, with counters to store the start and stop position along the line, perhaps with some adjustment of the reference level to take into account the brightness level. Arduino might manage all that if it's got several seconds after the ball goes through to do the calculations.

     

    Note this is just for discussion. I'm not offering it as a solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jc2048
    jc2048 over 10 years ago

    Rather than use a camera with it's very limited frame rate, you could use several linear sensor arrays like these:

     

    http://www.digikey.co.uk/product-detail/en/TSL1401CL/TSL1401CLCT-ND/3095283

     

    If you placed a wide angle lens, with a 90 degree field of view, in front of the device you'd have a fan-like view. One at each of the front corners, facing towards each other and up would give you the ability to do triangulation on a plane rising from the front. With another pair at the back, you'd then have enough information to do the timing and the trajectory. Wouldn't work for small objects, but might be ok for your tennis ball.

     

    They'd be much faster than a camera. You'd need a decent a/d. Haven't looked at sensitivity (adaption to varying light levels) and would have problems with background motion (people moving around) if it wasn't screened. Whether you could do all the processing with an Arduino I don't know - I would think not.

     

    Might not be necessary to digitise; if there were enough contrast between the ball and the background (enhance with a filter?) you could use a comparator, with counters to store the start and stop position along the line, perhaps with some adjustment of the reference level to take into account the brightness level. Arduino might manage all that if it's got several seconds after the ball goes through to do the calculations.

     

    Note this is just for discussion. I'm not offering it as a solution.