Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Measuring speed, angle and height
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 420 subscribers
  • Views 5107 views
  • Users 0 members are here
  • object
  • flying
  • angle
  • arduino
  • speed
  • height
Related

Measuring speed, angle and height

SGarciaV
SGarciaV over 11 years ago

Hi all,

 

I am discussing a possible project, but I am not certain how feasible it is. The project consists of using an Arduino, plus some sensor (or sensors) to measure the speed, angle and height of a flying object over a 6 x 30 cm surface. Although I am unfamiliar with the details, the object will pass over the surface and the Arduino needs to get how fast it is moving, the angle at which it crosses the surface and the distance from the surface to the object.

 

I posted a rough sketch below.

 

Can some one please provide some feedback as to how feasible this is and what sort of sensor(s) will be needed? Thanks! Salvador

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +1
    Here is a technique that might work - the accuracy depends on how well it is implemented. start with a narrow beam LED (preferably collimated) or a laser shine it through a section of a cylindrical lens…
  • SGarciaV
    SGarciaV over 10 years ago in reply to bhavikbhansali +1
    Hi Bhavik! Thank you for your reply. The object is a tennis ball traveling at approximately 70 to 90 miles per hour. Salvador
Parents
  • amgalbu
    amgalbu over 10 years ago

    HI Salvador

    what about two infrared barriers placed at a certain distance?

    The time it takes for the ball to travel from one barriers to the other gives you the speed, whereas the interrupted beams gives you the angle

     

    Cheers

    Ambrogio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to amgalbu

    Mmmm.... Ambrogio,

    your idea IMO arises at least a couple of issues. The first is that using beams, by definition these are not lasers but IR lights so for every barer there is a too wide acceptance range and consequently a precision loss. The second is that this means placing fixed position so there is not a full coverage or the real passage angle. I think that with this method you will try to use a well working system to manage a pre-defined targeting measurement system with a unknown behavioural system.

     

    Based on your suggestion - and ignoring the budget aspects as I don't know what are the costs for the  peripherals- maybe the idea of the IR measurement (as well as similar laser application) may work as it works at a specific wavelength range. The most reliable possibility I see to target the precise angle of passage is the use of a linear camera; there are some working well on the IR wavelength and other working in visibile light. Simple OpAmp band-pass filters can isolate only the desired wavelength, that will be the source light for measure. AFAIK (I used linear cameras about 25 years ago) these can be triggered as well as reading data without considering the acquired "images" but just the electric signal variation so I think that also a small micro controller board can do de job.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to amgalbu

    Mmmm.... Ambrogio,

    your idea IMO arises at least a couple of issues. The first is that using beams, by definition these are not lasers but IR lights so for every barer there is a too wide acceptance range and consequently a precision loss. The second is that this means placing fixed position so there is not a full coverage or the real passage angle. I think that with this method you will try to use a well working system to manage a pre-defined targeting measurement system with a unknown behavioural system.

     

    Based on your suggestion - and ignoring the budget aspects as I don't know what are the costs for the  peripherals- maybe the idea of the IR measurement (as well as similar laser application) may work as it works at a specific wavelength range. The most reliable possibility I see to target the precise angle of passage is the use of a linear camera; there are some working well on the IR wavelength and other working in visibile light. Simple OpAmp band-pass filters can isolate only the desired wavelength, that will be the source light for measure. AFAIK (I used linear cameras about 25 years ago) these can be triggered as well as reading data without considering the acquired "images" but just the electric signal variation so I think that also a small micro controller board can do de job.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • amgalbu
    amgalbu over 10 years ago in reply to balearicdynamics

    Hi Enrico

    An IR barrier detects objects that pass in front of the receiver, so the precision is not so bad

    I agree this is not the best solution but in my opinion is an option considered the limited computational resources available on the Arduino board

    Then if one decide to connect a camera that can automatically track objects to Arduino is a completely different approach...

     

    Cheers

    Ambrogio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to amgalbu

    Hi Ambrogio, it is true. I though to a series of single beams.

     

    About the camera instead, sure to manage data with a poor processing capabilities a hardware pre-processing circuit (cleaning the signal and isolating just what it is needed) maybe a good practice. The camera alone interfaced with the Arduino board ... I see it like an improbable challenge.

     

    Enrico