Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum OLED Screen that ISN'T low quality
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 415 subscribers
  • Views 1216 views
  • Users 0 members are here
  • devops
  • mod
  • oled
  • n64
  • animaton
  • console mod
  • dev
  • game console
  • arduino
Related

OLED Screen that ISN'T low quality

sivart3
sivart3 over 8 years ago

Hello All,

 

I have an issue, and have only recently found this site.  I believe you all may be able to help me if what I understand about this site is true.  I'm under the impression that this is a community site for programmers and engineers alike to discuss such topics.  I hope my discussion fits and and does not violate any terms, conditions or any site ethics in general.

 

I am trying to create a custom N64 (A Nintendo home gaming console which released in North America on September 26, 1996).  The front of the N64 has a panel with their logo on it about 2.3 x 1.5 inches in size.  Of course the unit I aim to produce will not be the same dimensions of the original N64, but I'd like to remain similar in size.  So what's my issue?

 

I'm trying to find a part I need, preferably 1 x 4 inches in size, why is this difficult?  Because I'm looking for an OLED screen of these dimensions.  I'm sure I'm just looking in all the wrong places, but the only ones I can find are super low quality.  I don't mean cost-wise either, I'm talking in terms of pixel/colours.  Most of what I can find have a very limited number of pixel available in the screen (such as 128 x 32) or they have just enough on the screen to provide the front operations of an alarm clock, and they all have between 1 & 8 colours. 

 

I'm looking for a OLED screen that can accommodate the animation I'll attach with a .gif on this post without having to remake it as an 8 or 16 bit animation.  I hope to have this screen come on when the console is on and continue to repeat the animation till it powers down.  The reason I want an OLED is because I REALLY want that black-black.  Like, in the space that the logo is not operating, I want it to look as black as I'm going to make the case of the console.

 

Could anyone PLEASE point me in the direction of someplace I could buy a screen like this?

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • BigG
    BigG over 8 years ago +3
    Have you looked at Adafruit's RGB OLED displays. I cannot vouch for those displays, but based on this quote from their website "and the contrast is very high (black is really black)" it may well be worth…
  • shabaz
    shabaz over 8 years ago +1
    Hi Nova, I think ebay/aliexpress is a possibility. The market for OLEDs seems to be for mobile phones and TVs etc., so you can probably pick up spares for a mobile phone if it is the correct size. The…
  • BigG
    BigG over 8 years ago +1
    I'm no expert in this area, but I think amoled displays offer the ppi you're after, although screen size may be an issue. Did a quick search online and pulled up this example https://marketplace.oled-info…
Parents
  • shabaz
    shabaz over 8 years ago

    Hi Nova,

     

    I think ebay/aliexpress is a possibility. The market for OLEDs seems to be for mobile phones and TVs etc., so you can probably pick up spares for a mobile phone if it is the correct size. The manufacturers don't produce them in many sizes, they concentrate on where they can make the most sales, so it's a matter of fitting your requirements to the nearest OLED display phone (as an example).

    They won't be easy to drive though, they need high-speed signals, and sometimes unusual voltages, and connectors with pins spaced less than half a millimetre apart. There's no off-the-shelf solution that I can think of.

     

    Had it been an LCD screen, then the chance of finding something practically usable is better, but the OLED options are more restrictive. But even then, something that is 1x4" sized is too unusual. Usually the ratio is something like 4:3, or a little wider, but 4:1 ratio is going to be hard. Did you mean 1x1.4"?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 8 years ago

    Hi Nova,

     

    I think ebay/aliexpress is a possibility. The market for OLEDs seems to be for mobile phones and TVs etc., so you can probably pick up spares for a mobile phone if it is the correct size. The manufacturers don't produce them in many sizes, they concentrate on where they can make the most sales, so it's a matter of fitting your requirements to the nearest OLED display phone (as an example).

    They won't be easy to drive though, they need high-speed signals, and sometimes unusual voltages, and connectors with pins spaced less than half a millimetre apart. There's no off-the-shelf solution that I can think of.

     

    Had it been an LCD screen, then the chance of finding something practically usable is better, but the OLED options are more restrictive. But even then, something that is 1x4" sized is too unusual. Usually the ratio is something like 4:3, or a little wider, but 4:1 ratio is going to be hard. Did you mean 1x1.4"?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • sivart3
    sivart3 over 8 years ago in reply to shabaz

    No, I actually am looking for a screen with dimensions of about 1 inch high and 4 inches wide, although I would settle for a screen that is 2 inches by 2 inches if I could find one.  That way I would just include the spinning logo and not the wording.

     

    When I check on eBay or AliE, all I can seem to find are screens with a very limited amount of pixels, such as a screen that's 128x32 pixels wide or 128x128 wide and it just wouldn't satisfy me to have a low quality picture to my build.  I did think about using the screen of a mobile phone I just worry about the size.  I don't know of any phone small enough to fit what I'm trying to do and I doubt I could trim one down.  I don't have any experience with OLED builds so I'm not going to say trimming one is impossible, though I highly doubt it is.