Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum mipi dsi on arduino?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 416 subscribers
  • Views 5268 views
  • Users 0 members are here
Related

mipi dsi on arduino?

haimbilia
haimbilia over 7 years ago

what is the best way to connect an arduino to a mipi dsi screen like this one:

https://www.alibaba.com/product-detail/1-2-inch-390-390-qhd_60814031531.html?spm=a2700.7724838.2017115.1.3a2a624eRDLpMO&…

can you connect the driver ic directly to arduino and just write a library? or do you need bridge controller?

is the arduino even fast enough to handle such screens?

i found very little information on mipi dsi. anyone know a good place to start?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +4
    This display seems to be used in the STM32L4R9I-DISCO - EVAL BOARD STM32L4R9I-DISCO - EVAL BOARD - there is quite a bit of info on the STMicroelectronics site . STM32L4R9I-DISCO Discovery Kit - Review
  • olibali
    olibali over 7 years ago in reply to lamming +1
    Hello. I know it is not an Arduino project but you could check this out: https://weekly-geekly.github.io/articles/444574/index.html He converts an SPI interface to MIPI DSI. He uses a flip flop to double…
Parents
  • lamming
    lamming over 7 years ago

    Did you sort this out.  I'm on the same track.  Appreciate any help. //Mik

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • olibali
    olibali over 7 years ago in reply to lamming

    Hello. I know it is not an Arduino project but you could check this out: https://weekly-geekly.github.io/articles/444574/index.html  He converts an SPI interface to MIPI DSI. He uses a flip flop to double the clock line and a resistor network to achive low speed and fast speed voltage levels. It requires higher clock rate so a simple 8MHz or 16MHz arduino won't/might not work. But a Bluepill (stm32 based arduino) or a Teensy should do the trick. I have just ordered a PCB to experiment with it, and to create a library.

     

     

    Hope it helped.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • olibali
    olibali over 7 years ago in reply to lamming

    Hello. I know it is not an Arduino project but you could check this out: https://weekly-geekly.github.io/articles/444574/index.html  He converts an SPI interface to MIPI DSI. He uses a flip flop to double the clock line and a resistor network to achive low speed and fast speed voltage levels. It requires higher clock rate so a simple 8MHz or 16MHz arduino won't/might not work. But a Bluepill (stm32 based arduino) or a Teensy should do the trick. I have just ordered a PCB to experiment with it, and to create a library.

     

     

    Hope it helped.