Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum USB to RS232
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 417 subscribers
  • Views 4387 views
  • Users 0 members are here
Related

USB to RS232

s1buell
s1buell over 7 years ago

Does anyone here have any experience with this topic?

 

I`m going from a TUSB2077APTRTUSB2077APTR controller to two FT232RL-REELFT232RL-REEL IC`s just to test this prototype idea.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago in reply to s1buell +7
    Hello Tom, I quite like FPGAs - but then that's what I do quite a bit. If this is a commercial project I could help you with FPGA design for money ! If not, then I'll be able to help a bit on E14 with…
  • michaelkellett
    michaelkellett over 7 years ago +6
    It looks as if you want an Arduino with 8 RS232 ports. The neatest way to do this is to use an FPGA - something fairly small will do. You can connect the FPGA to the Arduino via UART or SPI at logic level…
  • beacon_dave
    beacon_dave over 7 years ago in reply to s1buell +5
    "The idea is to connect 7 RS232 connections. Then access them via Arduino (or similar type proto board) in the end." Perhaps take a look at the ATxmega A1U or A3U family of AVR 8-bit microcontroller which…
Parents
  • michaelkellett
    michaelkellett over 7 years ago

    It looks as if you want an Arduino with 8 RS232 ports.

     

    The neatest way to do this is to use an FPGA - something fairly small will do. You can connect the FPGA to the Arduino via UART or SPI at logic level (care needed if it's a 5V Arduino).

     

    If you need true RS232 ports at correct levels then you'll need level shifters like the TI device you mentioned.

     

    The FPGA work will be challenging if you've never done any before, but you would be able to get true simultaneous operation of all 8 ports with buffering and good control of latency.

     

    If you are more used to processors consider using a fast ARM based part which will be able to do 8 UARTs in software at 9600 baud quite easily.

     

    As is so often the case, it would be much easier to make good suggestions if you would describe what you actually want to achieve in a bit more detail.

     

    For example, you might be able to use an ST Nucleo board (NUCLEO-F429ZI would be suitable)

    with a nice fast processor to do everything you need, including simulate 8 UARTS.

     

    MK

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 7 years ago

    It looks as if you want an Arduino with 8 RS232 ports.

     

    The neatest way to do this is to use an FPGA - something fairly small will do. You can connect the FPGA to the Arduino via UART or SPI at logic level (care needed if it's a 5V Arduino).

     

    If you need true RS232 ports at correct levels then you'll need level shifters like the TI device you mentioned.

     

    The FPGA work will be challenging if you've never done any before, but you would be able to get true simultaneous operation of all 8 ports with buffering and good control of latency.

     

    If you are more used to processors consider using a fast ARM based part which will be able to do 8 UARTs in software at 9600 baud quite easily.

     

    As is so often the case, it would be much easier to make good suggestions if you would describe what you actually want to achieve in a bit more detail.

     

    For example, you might be able to use an ST Nucleo board (NUCLEO-F429ZI would be suitable)

    with a nice fast processor to do everything you need, including simulate 8 UARTS.

     

    MK

    • Cancel
    • Vote Up +6 Vote Down