Arduino Forum ESP8266 03 Serial ESP 03 WiFi Module Wireless
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
  • Replies 1 reply
  • Subscribers 400 subscribers
  • Views 447 views
  • Users 0 members are here
  • arduino rf
  • arduino-robot
  • arduino uno
  • learn arduino
  • esp 03
  • esp8266
Related

ESP8266 03 Serial ESP 03 WiFi Module Wireless

Former Member
Former Member over 9 years ago

hello,

 

i am new to the use of arduino, and have some questions about the ESP 03

,

 

1>How does it work

 

2>are the GPIO pins in ESP 03 like the data pins on a transmitter reciever.

through which we can send/recieve  data ?

3>do the GPIO pins behave like channels in transmitter reciever,,,,???

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 9 years ago +3
    Hi Ashuman, The board behaves like a microcontroller (it has a microcontroller on-board). You can write a program or script for it, to control those pins or to read signal levels from those pins. It doesn…
Parents
  • shabaz
    shabaz over 9 years ago

    Hi Ashuman,

     

    The board behaves like a microcontroller (it has a microcontroller on-board).

    You can write a program or script for it, to control those pins or to read signal levels from those pins.

    It doesn't behave like some type of automatic wire - to - wireless modem/translater,

    not unless it is programmed to behave like that.

    The wireless is 802.11 (WiFi), and on top of that there are many protocols, including UDP or

    TCP on top of that. That is under control of your user program which you have to upload

    to the microcontroller.

    It is actually not as hard as it sounds, but needs some reading up, Adafruit/Sparkfun

    have some tutorials as I understand (but there are lots via google, these are

    just an example).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 9 years ago

    Hi Ashuman,

     

    The board behaves like a microcontroller (it has a microcontroller on-board).

    You can write a program or script for it, to control those pins or to read signal levels from those pins.

    It doesn't behave like some type of automatic wire - to - wireless modem/translater,

    not unless it is programmed to behave like that.

    The wireless is 802.11 (WiFi), and on top of that there are many protocols, including UDP or

    TCP on top of that. That is under control of your user program which you have to upload

    to the microcontroller.

    It is actually not as hard as it sounds, but needs some reading up, Adafruit/Sparkfun

    have some tutorials as I understand (but there are lots via google, these are

    just an example).

    • Cancel
    • Vote Up +3 Vote Down