Arduino Forum Input a signal from a sensor to an Arduino Due
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
  • State Suggested Answer
  • Replies 9 replies
  • Answers 5 answers
  • Subscribers 403 subscribers
  • Views 2311 views
  • Users 0 members are here
  • arduino
  • sensor
Related

Input a signal from a sensor to an Arduino Due

Former Member
Former Member over 11 years ago

I'm working with Arduino Due and I have a sensor that outputs a square signal with voltages in the range of 0-5V.

In the Due specs there is a warning that says:

"Warning: Unlike other Arduino boards, the Arduino Due board runs at 3.3V. The maximum voltage that the I/O pins can tolerate is 3.3V. Providing higher voltages, like 5V to an I/O pin could damage the board."

Is it possible to connect it to the board?

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 11 years ago +1 suggested
    Just put voltage divider on sensor output.... it will work great and about talk to sensor 3.3V logic is enough to drive logic1 on 5V sensor...
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hi Matt,

    There are level conversion modules available that will convert a 5 volt output sensor to 3.3 volt level. I do not know your exact application but you should be able to find a converter. The other options are to cut the voltage with a resistive divider or use 3.3 volt sensors.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to jw0752

    Thanks,

     

    And if the sensor also needs 5V to operate, can it be supplied by the Arduino Due?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to Former Member

    Yes, there is a 5V output on the Due as you can see in this picture, as long as your not drawing too much power

    ArduinoDue_Front.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to Former Member

    Yes, there is a 5V output on the Due as you can see in this picture, as long as your not drawing too much power

    ArduinoDue_Front.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer