Arduino Forum Reverse Footprint for Arduino Mega
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
  • State Not Answered
  • Replies 22 replies
  • Subscribers 400 subscribers
  • Views 7245 views
  • Users 0 members are here
  • arduino
  • arduino projects
Related

Reverse Footprint for Arduino Mega

colporteur
colporteur over 3 years ago

How do you mount a Mega on a PCB?

I'm using a Arduino Mega for a project and wanted to use Fritzing to create a PCB layout. The footprint for the Mega reflects the pinout of the motherboard. If I create a pin pattern on the board to mount the Mega directly to the board, then the pins need to be reversed. The Mega is flipped over and mounted face down on the PCB reversing the pinout.

I cannot find a pinout that reflects the Mega face down on a PCB. I would assume that is the way to install the board and not have a collection of jumpers running from the Mega board back to the PCB. If anyone has an insight I would welcome the input?

image

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 3 years ago +2
    I assume the PCB is plated through-hole? Put the footprint on the reverse of the PCB but actually solder the MEGA (or headers) onto the front of the board. That would work wouldn’t it?
  • BigG
    BigG over 3 years ago in reply to colporteur +2
    I would change the background colour so that you can see the white font. I did a quick test to prove and it is quite straightforward. If this is what you need, then I can place the modified fritzing…
  • BigG
    BigG over 3 years ago +1
    In PCB mode, click on the footprint and then change "pcb layer" to bottom.
Parents
  • colporteur
    0 colporteur over 3 years ago

    I stumbled on a work around to this question. The answer appears to the application. I took some screen shots of the Mega footprint while placing the component. I will attempt to explain my understanding.

    image

    The image far left is taken from Arduino webpage. The board has a few more pins than the Mega footprint in Fritzing but it will do for a visual representation of the Mega board.

    Image A is the Mega footprint found in Fritzing. The pin layout reflects the Arduino image shown. The image was imported while the View menu (second from left in red box), was set to View from Above.

    Image B is the Mega footprint with the View Menu was changed to View from Below.

    Both Image A and B are incorrect orientation for the Mega footprint. This is the reason I made this post.

    Image C is the Mega footprint imported while the View Menu is set to View from Below. If you were to look at a PCB from the below, the Mega would be on the other side of the PBB. This footprint orientation is correct. The pin asssignment labels would be correct if view from the bottom.

    Image D is the Mega footprint when View Menu is changed to View from Above. The orientation of the Mega is correct but the pin assignment labels are now incorrect.

    I plan to use Image C to layout a PCB. My plan is to send the board out to be made. I'm not confident the silk screening will be accurate.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • colporteur
    0 colporteur over 3 years ago

    I stumbled on a work around to this question. The answer appears to the application. I took some screen shots of the Mega footprint while placing the component. I will attempt to explain my understanding.

    image

    The image far left is taken from Arduino webpage. The board has a few more pins than the Mega footprint in Fritzing but it will do for a visual representation of the Mega board.

    Image A is the Mega footprint found in Fritzing. The pin layout reflects the Arduino image shown. The image was imported while the View menu (second from left in red box), was set to View from Above.

    Image B is the Mega footprint with the View Menu was changed to View from Below.

    Both Image A and B are incorrect orientation for the Mega footprint. This is the reason I made this post.

    Image C is the Mega footprint imported while the View Menu is set to View from Below. If you were to look at a PCB from the below, the Mega would be on the other side of the PBB. This footprint orientation is correct. The pin asssignment labels would be correct if view from the bottom.

    Image D is the Mega footprint when View Menu is changed to View from Above. The orientation of the Mega is correct but the pin assignment labels are now incorrect.

    I plan to use Image C to layout a PCB. My plan is to send the board out to be made. I'm not confident the silk screening will be accurate.