Arduino Forum L293d motor driver
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
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 400 subscribers
  • Views 2706 views
  • Users 0 members are here
Related

L293d motor driver

Kaushik_ma
Kaushik_ma over 3 years ago

So guys I had setup of rc car .I am using 4 motors , l293d driver ,ardunio Uno board and an hc -06 Bluetooth module for connection. The problem is after setting all if I supply current through batteries the l293d driver and ardunio is working but Bluetooth module is not working , instead I am giving the supply from power Bank the Bluetooth module and ardunio are running but l293d driver is not working..please tell me an solution

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 3 years ago +2 verified
    Can you show a photo or drawing of how power is connected?
  • ralphjy
    ralphjy over 3 years ago +2
    Have you tried removing the shield power jumper and powering the Arduino and the motors separately? You mentioned using a Power Bank. If this is a USB Power Bank, it will not power the motors (except…
  • shabaz
    shabaz over 3 years ago +2
    You're brave, constructing a battery pack from three LiPo cells that are unprotected according to the peeled one, into a cheap spring holder with thin wires. If there's a stall on the motors then expect…
Parents
  • ralphjy
    0 ralphjy over 3 years ago

    Have you tried removing the shield power jumper and powering the Arduino and the motors separately?

    image

    You mentioned using a Power Bank.  If this is a USB Power Bank, it will not power the motors (except for servo motors).  So it would make sense that your motors did not work.

    Without a connection schematic it is difficult to determine why the HC-06 isn't working when the battery is the power source.  It would be good to try a separate power source for the Arduino and the the motors, but make sure you remove the power jumper first!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ralphjy
    0 ralphjy over 3 years ago

    Have you tried removing the shield power jumper and powering the Arduino and the motors separately?

    image

    You mentioned using a Power Bank.  If this is a USB Power Bank, it will not power the motors (except for servo motors).  So it would make sense that your motors did not work.

    Without a connection schematic it is difficult to determine why the HC-06 isn't working when the battery is the power source.  It would be good to try a separate power source for the Arduino and the the motors, but make sure you remove the power jumper first!

    • Cancel
    • Vote Up +2 Vote Down