Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Looking for a small display recommendation
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 413 subscribers
  • Views 6686 views
  • Users 0 members are here
  • displays
  • model railroad
  • arduino projects
Related

Looking for a small display recommendation

colporteur
colporteur over 3 years ago

Does any member have a recommendation for a small display that is appropriate for scrolling from right to left?

After an hour culling the adafruit website with few returns, I have come to the E14 community hopefully to get a recommendation. I've been asked to build a two signs, one that scrolls "Welcome to Snow Island"  and the other "Thank you for Visiting Snow" Island. The signs will be positioned on top of a bridge on an HO scale model railroad layout.

I had hoped to use a MAX7219 Dot led Matrix MCU 8x32 but it is way to large for the foot print I have to work with. The bridge has a large flat surface about 4X4 inches to hold the sign.

Like any model railroad project cost is a factor. I don't have a big budget. I'm hoping to combine the display with an Nano Arduino to simulate a continuous text scrolling road sign to message visitors.

If your suggestions could contain the source for the part that would be great.

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 3 years ago +5
    Thank you for the input folks. Here are two displays I have ordered. If the displays on the left work it should be fairly simple to finish the project. Very little work on my part. The display on the right…
  • colporteur
    colporteur over 3 years ago in reply to colporteur +4
    community.element14.com/.../IMG_5F00_2289.MOV Do I buy or do I build? The S1144 (far left) displays arrived today. After installing the configuration software the display I wanted was working. At $10…
  • shabaz
    shabaz over 3 years ago in reply to beacon_dave +3
    Just saw these, look quite nice, just under 3.7" wide, available in many colors, and very cheap! However they either work for the use-case, or don't, since the behaviour of them is only configurable…
Parents
  • colporteur
    colporteur over 3 years ago

    image

    Thank you for the input folks. Here are two displays I have ordered. If the displays on the left work it should be fairly simple to finish the project. Very little work on my part. The display on the right require me to invest time in programming a pico. Something i have wanted to do for some time. With a project I have the motivation.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur over 3 years ago

    image

    Thank you for the input folks. Here are two displays I have ordered. If the displays on the left work it should be fairly simple to finish the project. Very little work on my part. The display on the right require me to invest time in programming a pico. Something i have wanted to do for some time. With a project I have the motivation.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Children
  • beacon_dave
    beacon_dave over 3 years ago in reply to colporteur
    colporteur said:
    The display on the right require me to invest time in programming a pico.

    Looks like there is some code out there for Arduino if you want to start out with the Nano.

    https://github.com/MartyMacGyver/LCD_HT1622_16SegLcd

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to beacon_dave

    SOLD BD! Love you man.

    I  made a list of retirement stuff I am involved with. I then divided the list between short term and long term commitments. It seems I have made so many long term (multiple days over multiple weeks) I don't have cycles for short term projects.

    I need this to be a quick in and out. If the unit on the left works it should be quick. It talks about using a windows app to configure. I'm not sure what that involves. Hopefully it is just enter text here, what mode and upload. We will see.

    Again man, thanks for the resource.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to colporteur

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    Do I buy or do I build? The S1144 (far left) displays arrived today. After installing the configuration software the display I wanted was working. At $10 per unit which includes the shipping. It was a cost effective solution.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to colporteur

    Nice-looking display! I'm tempted to buy one or two of these, could come in handy for projects, perhaps with a bit of adaptation.