Arduino
  • Products
  • More
Arduino
Documents Tutorial FRDM-KL25Z & ARDUINO: Freescale Freedom Zumo Robot
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: FreescaleTools_and_Software
  • Date Created: 8 Feb 2013 11:50 AM Date Created
  • Last Updated Last Updated: 1 Nov 2016 9:21 PM
  • Views 1418 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Tutorial FRDM-KL25Z & ARDUINO: Freescale Freedom Zumo Robot

This tutorial was extracted from Erich Styger blog http://mcuoneclipse.wordpress.com with his agreement.

image image

   

The cool thing with the Freedom board is: there are many exciting Arduino boards out there which want to be used with the FRDM-KL25Z. I have spent most of my last week-end with creating a little black beauty:

  

    

FRDM Zumo Robot

FRDM Zumo Robot

  

  

 

When I was looking for some nice DC motors with quadrature encoders for my next lecture project, I stumbled over the Pololu web site which had *exactly* the DC motors I was looking for. And their Zumo Robot Robot Kit was something which attracted my eyes.

  

   

I always joked :roll: about women shopping habits. But my wife is right: If it is about electronics, I’m not different at all :grin:

  

  

That robot is smaller than 10 cm on each size, so it qualifies as a Mini-Sumo. Although I have a different purpose in mind for my robot…..

  

  

Chassis and Motors

     

I ordered the chassis with two 75:1 Micro High Performance Metal Gearmotors which enable the chassis to move about 50 cm in a second. The chassis includes a battery compartement on the bottom for 4 AA batteries (so up to 6V):

     

   

Zumo Chassis with DC Motors

Zumo Chassis with DC Motors

 

    

:idea: I did *not* follow the Pololu instructions to solder the motor with the Arduino shield: instead I used flexible wires to attach the motors to the board. That allows me to change motors or disassemble the kit in a much simpler way.

  

   

Arduino Board

   

The Arduino board comes with a few parts unpopulated (Buzzer, Headers, Switches). The board features a tiny (but powerful) Dual Full-H Bridge, a Buzzer, Battery Voltage Sensing and a I2C Accelerometer+Magnetometer sensor:

  

  

Zumo Arduino Board

Zumo Arduino Board

  

  

Freedom Board

  

The  FRDM-KL25ZFRDM-KL25Z needs to connected‘face down to the Zumo board I plan to layout an intermediate PCB with my to-be-added hardware But for now I’m using normal breakable header rows as‘interconnection This is necessary as otherwise the Freedom board is very close to the Zumo board components

   

  

Headers to increase distance between boards

Headers to increase distance between boards

   

   

Power Supply

   

The  FRDM-KL25ZFRDM-KL25Z is powered from the batteries through P5-9VIN But the Freedom board only generates the 3.3V from P5-9VIN and but not the needed 5V to the header(see this post). That 5V is needed by the Shield. So for now I’m using a rather bulky DC-DC converter and supply the needed 5V from the battery to the USB 5V supply line, until I can replace the DC-DC converter with a smaller one. At least everything is working now :-) .

   

   

Software, and Next Steps

   

The software in CodeWarrior with Processor Expert is ready for most parts. Motors (speed/direction), LED’s and Buzzer are working. Magnetometer/Accelerometer and Battery Voltage Sensing are in progress. The current software is available on GitHub with all the Processor Expert components. And: I have a Bluetooth module ready to integrate, plus I want to add a line scanning module too. So enough fun for a couple of dark nights and week-ends :-) .

    

  

FRDM Zumo backside

FRDM Zumo backside

   

   

Happy Zumoing :-)

  • tutorial
  • avr
  • microchip
  • hardware
  • cortex-m0+
  • sports_technology
  • freescale
  • robots
  • Cortex-M
  • kinetis
  • robot
  • cortex
  • embedded
  • frdm-kl25z
  • stm32
  • Design
  • kinetis-l
  • prototyping
  • platform
  • cortex-m0
  • arduino_development_environment
  • arm
  • arduino
  • freedom
  • pic
  • atmel
  • Share
  • History