Arduino
  • Products
  • More
Arduino
Documents Getting started with stepper motors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 28 Feb 2014 12:30 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 7:49 AM
  • Views 911 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Getting started with stepper motors

i am a beginner and am trying to learn and understand electronics 

few days backs i was playing around with my arduino uno r3 kit ( ordered for US$ 29 )

 

it came with this 5V  stepper motor ( part number  28BYJ- 48 ) ( easily found on ebay and very cheap )

the same can be found with 12V

imageimage

i found this motor very easy to use and control using arduino uno r3 

  • Speed Variation Ratio : 1/64
  • Stride Angle : 5.625° /64
  • one complete rotation is 4096 steps 

 

 

this motor needs a ULN2003 Driver Board which is again very simple to use , understand and even make yourself

it can be very easily found on ebay for very cheap ( around US$ 2 )

Fullscreen contentimage_76497.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

you will find the set for less then US$ 5 on ebay

 

connection of the driver board with arduino is also simple just the 4 pins for the arduino which are set in the program will connect to the in1 in2 in3 and in4 

you have to connect 5V or 12V (depending on the motor ) and ground to the driver board as the motor doesnt run safely on power from arduino

the 5V motor does run but i have found people saying its not safe 

 

the program required to run the motor can be found in the examples in the arduino software  its very easy to understand, the program is written with explanation so you can just read through, the program can be modified to do exactly what you want maybe add a switch maybe add a sensor

it just takes 3 4 hours (as a beginner) to get used to it 

 

you can also read the link below it has the details about the motor and the driver board and an example program which can also be used on arduino

http://www.geeetech.com/wiki/index.php/Stepper_Motor_5V_4-Phase_5-Wire_%26_ULN2003_Driver_Board_for_Arduino

 

hope i was helpful

  • getting_started
  • stepper-motor
  • arduino
  • Share
  • History