Arduino
  • Products & Partners
  • More
Arduino
Polls What Motor Driver is Best for Arduino?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: electronicslearner101
  • Date Created: 7 Jul 2021 4:58 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:00 PM
  • Views 2348 views
  • Likes 1 like
  • Comments 5 comments
Related
Recommended

What Motor Driver is Best for Arduino?

I am wanting to create a WiFi car but I am debating on what motor driver to use…I want to use it with my Arduino Uno or ESP32.

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dougw
    dougw over 5 years ago +5
    Part Efficiency L298N 30-70% L293 50-90% TB6612 91-95%
  • koudelad
    koudelad over 5 years ago +3
    I would personally start with the mechanical design and selecting the motors - it is hard to choose a motor driver without any additional information.
  • colporteur
    colporteur over 5 years ago in reply to electronicslearner101 +3
    If I can rephrase koudelad comment, define "Best"? Your follow-up post defined "Best" as efficiency That provided dougw the insight to enable a response of other.
  • robogary
    robogary over 5 years ago

    For a "smart car"  depends on the motor voltage, motor amps (and stall current), and if you want to use motor encoders.

     

    The L298N are good for 12V 2 amps, easy to interface to different controllers.

    The L293D is 1.2A peak.

     

    My Power Wheels cars with Arduino controls, use these H bridges:

    IBT-4 (5-15V/50A) H-bridge High-power Motor Driver Module Smart Car. This H bridge works exactly the same as

    L298N Motor Driver, but obviously has alot more oomph.

    These run open loop voltage control, same as L298N. 

     

    For Arduino MKR1000 smart car, this shield is good for using encoder feedback. (but a bit pricey. So are the gearmotors with encoders). https://store.arduino.cc/usa/mkr-motor-carrier

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 5 years ago in reply to electronicslearner101

    If I can rephrase koudelad comment, define "Best"?

     

    Your follow-up post defined "Best" as efficiency That provided dougw the insight to enable a response of other.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 5 years ago

    Part       Efficiency

    L298N   30-70%

    L293      50-90%

    TB6612  91-95%

     

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • electronicslearner101
    electronicslearner101 over 5 years ago in reply to koudelad

    Hi there. I am using 5-12v DC Motors. I have the mechanical design made and it can hold any of these drivers. I am just debating which one is the most efficient for my 5-12V DC Motors I should have specified. Thanks!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • koudelad
    koudelad over 5 years ago

    I would personally start with the mechanical design and selecting the motors - it is hard to choose a motor driver without any additional information.

    • Cancel
    • Vote Up +3 Vote Down