Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General What am I missing here to boot the kernel and mount root file system for AVNET MicroZed board - how to debug here?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 373 subscribers
  • Views 932 views
  • Users 0 members are here
  • ZedBoard General Questions
  • Software Application Development
  • Zedboard Training
Related

What am I missing here to boot the kernel and mount root file system for AVNET MicroZed board - how to debug here?

dexterous.me82
dexterous.me82 over 6 years ago

I have an AVNET microzed board  PB-AES-Z7MB-7Z010-G board.

It just says "Starting kernel ..." and I don't see anything further.

How do I see all the logs? I don't know why it is stopped like - "Starting Kernel..."?

 

From where this print is coming and why I can't see any more logs?

 

Here are the logs -

 

 

U-Boot 2013.01-dirty (Jun 14 2013 - 16:25:48)

 

 

DRAM:  512 MiB

WARNING: Caches not enabled

MMC:   zynq_sdhci: 0

SF: Detected S25FL129P_64K with page size 64 KiB, total 16 MiB

In:    serial

Out:   serial

Err:   serial

Net:   Gem.e000b000

Hit any key to stop autoboot:  0

Copying Linux from SD to RAM...

Device: zynq_sdhci

Manufacturer ID: 1b

OEM: 534d

Name: 00000

Tran Speed: 50000000

Rd Block Len: 512

SD version 2.0

High Capacity: No

Capacity: 971.5 MiB

Bus Width: 4-bit

Loading bitstream from SD/MMC/eMMC to RAM..

Device: zynq_sdhci

Manufacturer ID: 1b

OEM: 534d

Name: 00000

Tran Speed: 50000000

Rd Block Len: 512

SD version 2.0

High Capacity: No

Capacity: 971.5 MiB

Bus Width: 4-bit

reading system.bit.bin

2083740 bytes read in 289 ms (6.9 MiB/s)

reading uImage

4162648 bytes read in 570 ms (7 MiB/s)

reading devicetree.dtb

7370 bytes read in 12 ms (599.6 KiB/s)

reading uramdisk.image.gz

2379781 bytes read in 329 ms (6.9 MiB/s)

## Booting kernel from Legacy Image at 03000000 ...

   Image Name:   Linux-4.19.0-xilinx-v2019.1

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    4162584 Bytes = 4 MiB

   Load Address: 00008000

   Entry Point:  00008000

   Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at 02000000 ...

   Image Name:   core-image-minimal-microzed-zynq

   Image Type:   ARM Linux RAMDisk Image (uncompressed)

   Data Size:    2379717 Bytes = 2.3 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 02a00000

   Booting using the fdt blob at 0x02a00000

   Loading Kernel Image ... OK

OK

   Loading Ramdisk to 1f910000, end 1fb54fc5 ... OK

   Loading Device Tree to 1f90b000, end 1f90fcc9 ... OK

 

 

Starting kernel ...

  • Sign in to reply
  • Cancel
  • drozwood90
    drozwood90 over 6 years ago

    HI there,

     

    Are you using the PetaLinux image we created, or the Yocto image you mentioned in another thread?

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • narrucmot
    narrucmot over 6 years ago

    The boot messages are buffered, so it is sometimes very difficult to tell where *exactly* the kernel has hung during boot.  One thing I can think of is to make sure the "partition" size definitions in the u-boot config (for the kernel, ramdisk, dtb, etc.) are at least as large as the kernel, ramdisk, and dtb files.  If you have a tftp server you could try pausing u-boot and boot the system via tftpboot instead.

     

    Or, better yet, download and install a known-good PetaLinux BSP:
    MicroZed

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dexterous.me82
    dexterous.me82 over 6 years ago in reply to drozwood90

    Can you please point out to me to building  PetaLinux  for my AVNET MicroZEd board?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bhfletcher
    bhfletcher over 6 years ago in reply to dexterous.me82

    Go to MicroZed --> Reference Designs --> PetaLinux Board Support Packages