Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Trying to create in PetaLinux 2018.3 rootfs.ext4 image.ub and BOOT.bin of UltraZed-3EG-IO-Card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 367 subscribers
  • Views 372 views
  • Users 0 members are here
  • ZedBoard General Questions
  • Ultrazed Hardware Design
Related

Trying to create in PetaLinux 2018.3 rootfs.ext4 image.ub and BOOT.bin of UltraZed-3EG-IO-Card

sint12345
sint12345 over 6 years ago

Hi,

 

As I understand that I must first create a project in PetaLinux' as this step reads the new board bsp that it is ultrazed-3eg-io-card

 

After I done those steps, I got the following Error:

IOError: [Errno 2] No such file or directory: '/tools/PetaLinux2018.3/petalinux/ultrazed_debug_board/uz3eg_iocc_2018_2/project-spec/meta-user/recipes-core/images/petalinux-image-full.bbappend'

 

 

 

 

Our FW Engineer wrote the following procedure:

 

Sourcing

3.2.1. ‘cd petalinux’

3.2.2. in the project folder: ‘source settings.sh’

3.3. Create Project

3.3.1. ‘mkdir microsoft_debug_board’

3.3.2. ‘cd microsoft_debug_board’

3.3.3. create new project from xilinx bsp:

‘petalinux-create -t project -s

../debug_board_config/xilinx-ultra96-reva-v2018.3-final.bsp’

3.3.4. cd xilinix-ultra96-reva-2018.3

3.4. Build

3.4.1. ‘petalinux-build’

 

So I got to 3.4.1 and it stacked

 

 

Thanks in advance,

 

Shiri

Attachments:
7167.history_create_prj.log.zip
  • Sign in to reply
  • Cancel
  • narrucmot
    narrucmot over 6 years ago

    Hi Shiri,

     

    Thank you for attaching the log file.  That was helpful.  A significant clue to what may be the issue you of your failed PetaLinux build are these warning messages:

    WARNING: Your PetaLinux project was last modified by PetaLinux SDK version "2018.2",

    WARNING: however, you are using PetaLinux SDK version "2018.3".

     

    It is strongly advised that the version of PetaLinux BSP *must match* the installed PetaLinux tools version.  In this case PetaLinux 2018.2.  If you also plan to make changes to the underlying hardware platform then Vivado 2018.2 will also be required.