Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Ultrazed vcu trd 2019.2 add SDI RX problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 375 subscribers
  • Views 2890 views
  • Users 0 members are here
Related

Ultrazed vcu trd 2019.2 add SDI RX problem

pierlum
pierlum over 6 years ago

Hello,

I follow the flow from impleting to building petalinux images of ultrazed vcu trd 2019.2 design and it works. I modified the vivado project adding the SDI RX part from zcu106 vcu trd design and I edited device tree adding the entryn for sdi rx part. But in petalinux running on the board I can't find the sdi rx devices. What's I'm wrong?

Thank you very much.

 

https://xterra2.avnet.com/xilinx/zedboard/ultrazed-ev/vcu-trd-ports/rdf0428-uz7ev-vcu-trd-2019-2

  • Sign in to reply
  • Cancel

Top Replies

  • drozwood90
    drozwood90 over 6 years ago +1
    Have you included this in the device tree? --Dan
  • drozwood90
    drozwood90 over 6 years ago in reply to pierlum +1
    The SDI device. I've not personally built the 2019.2 design at this time, but PetaLinux always needs devices to be defined. For example, in SDSoC you have to add: /{ xlnk { compatible = "xlnx,xlnk-1.0…
  • drozwood90
    drozwood90 over 6 years ago in reply to pierlum +1
    HI there, Next time, try using "Quote" or "Syntax Highlighting". That will make this more clear to read. Second, have you compared that to the files that come as part of the example? --Dan
Parents
  • drozwood90
    drozwood90 over 6 years ago

    Have you included this in the device tree?

     

    --Dan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 5 years ago in reply to drozwood90

    Hello,

     

    I create a project with Vivado. And export xsa file. I need a .bsp file.

    I am using Vivado/Vitis 2019.2. How can I create a .bsp file ? Should I write it myself ?

    I want to use this .bsp file with petalinux-create command.

     

    Thanks for reply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • narrucmot
    narrucmot over 5 years ago in reply to e14 Contributor

    The .bsp file is a product of the petalinux-package command, which is run after first successfully completing the steps to create, configure, and build the PetaLinux project.

     

    You can get an idea of the steps involved by looking at the BSP build scripts for the Avnet UZ7EV SOM (with EV carrier) in Avnet's petalinux github repository:

    https://github.com/Avnet/petalinux/blob/2020.2/scripts/make_uz7ev_evcc_base.sh

    https://github.com/Avnet/petalinux/blob/2020.2/scripts/common.sh

     

    You may also want to look at Xilinx UG1144 - PetaLinux Tools Documentation Reference Guide

     

    --Tom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • narrucmot
    narrucmot over 5 years ago in reply to e14 Contributor

    The .bsp file is a product of the petalinux-package command, which is run after first successfully completing the steps to create, configure, and build the PetaLinux project.

     

    You can get an idea of the steps involved by looking at the BSP build scripts for the Avnet UZ7EV SOM (with EV carrier) in Avnet's petalinux github repository:

    https://github.com/Avnet/petalinux/blob/2020.2/scripts/make_uz7ev_evcc_base.sh

    https://github.com/Avnet/petalinux/blob/2020.2/scripts/common.sh

     

    You may also want to look at Xilinx UG1144 - PetaLinux Tools Documentation Reference Guide

     

    --Tom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 5 years ago in reply to narrucmot

    Hello,

     

    But there is command like    petalinux-create -t project -s .....bsp

    if I dont have .bsp file i can not use this command.

     

    Thanks,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • narrucmot
    narrucmot over 5 years ago in reply to e14 Contributor

    Use the "petalinux-create -t project -s <PATH-TO-BSP>" command only when using a pre-built BSP as the starting point of your PetaLinux development.

     

    When starting a PetaLinux project from scratch the command is more like:

    $ petalinux-create --type project --template zynqMP --name <petalinux_project_name>"

     

    Followed by the command to import the .xsa file for your Vivado hw project:

    $ petalinux-config --silentconfig --get-hw-description=<path/to/xsa_file> -p </path/to/petalinux_project>

     

    Then follow the rest of the steps described in Xilinx UG1144 and in the Avnet build scripts to build the OS image and package the PetaLinux project into a .bsp file.

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 5 years ago in reply to narrucmot

    Hello,

     

    According to UG1144, I've done

    petalinux-create --type project --template zynqMP --name <project_name>"

    petalinux-config --silentconfig --get-hw-description=<path/to/xsa_file>

    petalinux-build

    petalinux-package --boot  ....

     

    After these commands all images/linux folder files cretaed. That's ok. But when I boot from SD card (putting BOOT.bin and image.ub), Then I look in serial port with TeraTerm, there is no written lines, and after a while ps_err_out led is red.

     

    Also when I look at the "/project-spec/meta-user/recipes-bsp/device-tree/files/" folder and in this folder there is 2 empty files (pl-custom.dtsi & system-user.dtsi). Should I write anything to dtsi files before any petalinux commands

     

     

    Thanks,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • narrucmot
    narrucmot over 5 years ago in reply to e14 Contributor

    You may need to configure your PetaLinux project for the correct boot UART and boot media settings.

     

    It may also be helpful to compare the project configuration settings to a known-good PetaLinux project like that for the TRD you mentioned previously or one of the pre-built BSPs that can be downloaded here:

    https://avnet.me/zedsupport

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 5 years ago in reply to narrucmot

    Hello,

     

    When I look at the "/project-spec/meta-user/recipes-bsp/device-tree/files/" folder and in this folder there is 2 empty files (pl-custom.dtsi & system-user.dtsi)

    I thinks this was the problem. Should I write anything to .dtsi files before petalinux-build command ?

    For example ;

     

    &amba_pl {

    vcu_apm: apm@0xa0140000 {

    #address-cells = <0x1>;

    #size-cells = <0x1>;

    compatible = "generic-uio";

    reg = <0x0 0xa0140000 0x0 0x10000>;

    reg-names = "generic";

    };

    };

     

     

    &amba_pl {

    xlnk {

    compatible = "xlnx,xlnk-1.0";

    };

    };

     

    Like these.

     

    Thanks,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • narrucmot
    narrucmot over 5 years ago in reply to e14 Contributor

    It is usually not necessary to write anything to the pl-custom.dtsi file. 

     

    It is sometimes necessary to write peripheral configuration/descriptions in the system-user.dtsi file.  Take a look at Avnet's system-bsp.dtsi file for the UltraZed-EV SOM + EV carrier:

    https://github.com/Avnet/meta-avnet/blob/2020.2/recipes-bsp/device-tree/files/uz7ev-evcc/system-bsp.dtsi

     

    There is a lot in this file - perhaps more than you need.  This is just an example of what is sometimes needed, and it is very dependent on the PS and PL configuration for your design.

     

    --Tom