Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Writing value on a pin on Zynq 7020
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 371 subscribers
  • Views 607 views
  • Users 0 members are here
  • picozed 7020
  • zynq 7000
  • fmc carrier card
Related

Writing value on a pin on Zynq 7020

steven01
steven01 over 6 years ago

Hello,

I have been struggling with writing a value to a pin on Zynq 7020. I have been using PicoZed SOM 7020 along with the FMC carrier card v2. My intention is to toggle the D10 PS_LED. I have gone through the documentation to the PicoZed SOM and FMC carrier card v2 and I have found that the D10 PS_LED is connected to the pin 40 on connector JX3. Which is then connected to the Zynq Pin B14 (MIO Bank 501).

My question is what pin number shall I pass into the XGpioPs_SetDirectionPin and XGpioPs_WritePin functions to be able to blink the LED? I have used 47 but it does not work. Can anybody tell me how to convert B14 into pin number for above mentioned functions?

  • Sign in to reply
  • Cancel
  • bhfletcher
    bhfletcher over 6 years ago

    Pin B14 is MIO #47. You can see this in the PicoZed schematic, but that is derived from the Xilinx specification for the device pinout.

    https://www.xilinx.com/support/packagefiles/z7packages/xc7z020clg400pkg.txt

    Pin  Pin Name Memory Byte Group  Bank  VCCAUX Group  Super Logic Region  I/O Type  No-Connect 

    B14 PS_MIO47_501 NA 501 NA NA MIO NA

     

    So, 47 is correct, but that isn't working for you. It's possible you missed some of the setup steps. There is a series of really excellent articles called MicroZed Chronicles http://adiuvoengineering.com/microzed-chronicles/ . I suggest you check out #10 and see if that helps.

    https://forums.xilinx.com/t5/Xcell-Daily-Blog-Archived/Driving-the-Zynq-SoC-s-GPIO-Adam-Taylor-s-MicroZed-Chronicles/ba-…

     

    Bryan