Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General SD card IO errors
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 372 subscribers
  • Views 411 views
  • Users 0 members are here
Related

SD card IO errors

e14 Contributor
e14 Contributor over 14 years ago


I have started to get massive amounts of IO errors on the SD card and generally erratic behavior.

I've resorted to clearing the partition table and rebuilding it.  That was also erratic.  Formatting throws a bunch of errors as well. 

At this point, I have a wiped SD card.  I did copy the files in the first partition to a backup usb disk (that has zero issues).

Is there supposed to be more than one partition on the SD Card?  fdisk thought that there were four.

I'd like to get back to a clean setup.  Hopefully the backup I have of the file from the one partition are valid...

Is there a description of the SD configuration (image?) somewhere?

Thanks,
Greg

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    The original CF that comes with the zedboard contains a single fat32 partition and if you have back-upped the files is sufficient that you reformat the whole CF in fat32, copy the 5 files and you're done! 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor


    8GB "30MB/s" card and everything is working okay for the moment.

    Cheers,
    Greg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    We have a few zedboards here and none of the SD cards are working properly... Seems to be some cheap memory...
    Even after wiping the SD card and copying the xillinux image onto it the I/O errors continued.
    I also use Sandisk, 8 GB 30MB/s, and there are no I/O errors.