Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Zedboard CTT
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 372 subscribers
  • Views 579 views
  • Users 0 members are here
Related

Zedboard CTT

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I'm working through the Concepts Tools and Techniques document (CCT) for Vivado 2013.2. 

I got as far as Page 33.  In Step 3 of 3.1.1, it says to use the Zedboard Development Template preset to restore the Zynq PS to the default settings.  I do this, click on OK in a few spots, but the block diagram remains unchanged.  In order to get it to do what I believe is being asked, I have to delete the block, and then continue with the exercise.

Then, I get as far as Figure 3-3.  The GPIO_1[0:0] does not appear.  I also cannot get MIO[53:0] to appear.

Any ideas what I'm doing wrong?

Thanks

Brian

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I figured out why the ports weren't appearing.  There are some tiny buttons on the processor block that must be clicked to expand the ports.  So, I found those.

    Still don't know why the template doesn't work.

    So, on to the software.  Copied from the PDF file into the C source file.  Three compiler errors:

    inbyte() doesn't seem to be defined.  I see it in a header, but not a library file.

    XPAR_PS7_GPIO_1_DEVICE_ID is not defined, but XPAR_PS7_GPIO_0_DEVICE_ID is defined.

    Similarly, XPAR_PS7_SCUGIC_1_DEVICE_ID is not defined,
    but XPAR_PS7_SCUGIC_0_DEVICE_ID is.

    Correcting for the above by
    #define inbyte getchar
    and replacing what is not defined by what is, the program immediately terminates when it is run.  Nothing gets printed to the terminal screen.

    Ideas?

    Thanks.  Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I figured out why the ports weren't appearing.  There are some tiny buttons on the processor block that must be clicked to expand the ports.  So, I found those.

    Still don't know why the template doesn't work.

    So, on to the software.  Copied from the PDF file into the C source file.  Three compiler errors:

    inbyte() doesn't seem to be defined.  I see it in a header, but not a library file.

    XPAR_PS7_GPIO_1_DEVICE_ID is not defined, but XPAR_PS7_GPIO_0_DEVICE_ID is defined.

    Similarly, XPAR_PS7_SCUGIC_1_DEVICE_ID is not defined,
    but XPAR_PS7_SCUGIC_0_DEVICE_ID is.

    Correcting for the above by
    #define inbyte getchar
    and replacing what is not defined by what is, the program immediately terminates when it is run.  Nothing gets printed to the terminal screen.

    Ideas?

    Thanks.  Brian