Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Zedboard CTT
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 372 subscribers
  • Views 580 views
  • Users 0 members are here
Related

Zedboard CTT

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I'm working through the Concepts Tools and Techniques document (CCT) for Vivado 2013.2. 

I got as far as Page 33.  In Step 3 of 3.1.1, it says to use the Zedboard Development Template preset to restore the Zynq PS to the default settings.  I do this, click on OK in a few spots, but the block diagram remains unchanged.  In order to get it to do what I believe is being asked, I have to delete the block, and then continue with the exercise.

Then, I get as far as Figure 3-3.  The GPIO_1[0:0] does not appear.  I also cannot get MIO[53:0] to appear.

Any ideas what I'm doing wrong?

Thanks

Brian

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Ok.  Started with a clean project this time instead of working from HelloWorld.  That seemed to take care of several things:
    1)  No problems with using the template definition for the Zedboard Zynq.
    2)  When I got to the SDK, the inbyte() function finally found its source, so I didn't have to use the macro.

    However, I still had to change the 1s to 0s for the two device ID constants:
    XPAR_PS7_SCUGIC_1_DEVICE_ID
    XPAR_PS7_GPIO_1_DEVICE_ID

    Then the whole thing worked like a champ.

    My block diagram doesn't look exactly like the diagram in the .pdf.  Specifically, there are some extra unconnected ports and pins, and some missing ports and pins. 

    Ahh well ... to be investigated another day.

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Ok.  Started with a clean project this time instead of working from HelloWorld.  That seemed to take care of several things:
    1)  No problems with using the template definition for the Zedboard Zynq.
    2)  When I got to the SDK, the inbyte() function finally found its source, so I didn't have to use the macro.

    However, I still had to change the 1s to 0s for the two device ID constants:
    XPAR_PS7_SCUGIC_1_DEVICE_ID
    XPAR_PS7_GPIO_1_DEVICE_ID

    Then the whole thing worked like a champ.

    My block diagram doesn't look exactly like the diagram in the .pdf.  Specifically, there are some extra unconnected ports and pins, and some missing ports and pins. 

    Ahh well ... to be investigated another day.

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi Brian.
       Have you solved the promblem?(XPAR_PS7_SCUGIC_1_DEVICE_ID not declared) Would you like to share the solution?
       Thanks.
       May.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Changing the constant allowed the example code to compile and run.  I was told that the ISE tools used a different indexing scheme than the Vivado tools, but the labels for the constants weren't changed in the source c code.

    Brian