Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Xillinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 373 subscribers
  • Views 730 views
  • Users 0 members are here
Related

Xillinux

deaxman
deaxman over 13 years ago

In order to use Xillinux and Xillybus to moniter registers through the linux command terminal with /dev/something what do I have to do on the FPGA side, I figure I need to add the Xillybus IP but each time I load the bit file with impact it shuts down the PS (Xillinux) side and the logo disappears.  How can I load a design, (e.g. switch on --> led on is a common one) and have the terminal tell me the state of the switches?  Any documentation on this or examples?  I've read all of the xillinux documentation and it helped on the Xillinux side but nothing on the PL side or about creating a custom bit file and reading the registers defined in the HDL code used to create it.  Thanks a ton!

  • Sign in to reply
  • Cancel
Parents
  • deaxman
    0 deaxman over 13 years ago

    So to do this I should modify Xillydemo.v?  They say add extra hdl files but synthesis to a bit file only uses one hdl file right?  So I either need to replace or change xillydemo but it has the IP connections etc in it so it seems like changing it is the only alternative?  Is this true?  Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • deaxman
    0 deaxman over 13 years ago

    So to do this I should modify Xillydemo.v?  They say add extra hdl files but synthesis to a bit file only uses one hdl file right?  So I either need to replace or change xillydemo but it has the IP connections etc in it so it seems like changing it is the only alternative?  Is this true?  Thanks!