Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Ethernet is not running in Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 373 subscribers
  • Views 3770 views
  • Users 0 members are here
Related

Ethernet is not running in Zedboard

e14 Contributor
e14 Contributor over 13 years ago

I was trying to migrate the WinCE BSP for Xilinx ZC702 for ZedBoard and got stuck in getting the Ethernet working.
After I change the PHY address to 0 it successfully completes the autonegotiation and reports the link speed. There after it fails and looks like it is not receiving any frames.
I blamed the PHY chip differences and spend couple of days in the data sheets and no luck. At that point I thought of trying with the supplied Linux boot image(till then I used the xilinx XPS and run the sample based on the hw definition file from Zedboard and didn't check the LAN).
Surprisingly it didn't even do the self pinging, I changed the IP address but it stuck with the ping command as follows
PING 192.168.1.10 (192.168.1.10): 56 data bytes

Out of the 3 boards we have I checked two and got the same results. Any help is much appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • zedhed
    zedhed over 13 years ago +1
    Hi Seetharam, We have a Getting Started Guide posted in the Documents section on ZedBoard.org which contains a section on using the ZedBoard Ethernet. http://zedboard.org/sites/default/files/documentations…
Parents
  • zedhed
    0 zedhed over 13 years ago

    Seetharam,

    I am glad that we are both seeing the same behavior even though it might not be the expected behavior.

    I don't think that there were any changes made within the Ethernet driver itself for ZedBoard.  I would suggest taking a look at the device tree entry for the Ethernet driver and see if there are any differences from the device tree entry used for ZC702. 

    This may help you isolate a chip specific setting that you might need for your BSP code.

    Here is the Ethernet device entry for ZedBoard out-of-box demos:

    eth@e000b000 {
        compatible = "xlnx,ps7-ethernet-1.00.a";
        reg = <0xe000b000 0x1000>;
        interrupts = <0x0 0x16 0x0>;
        interrupt-parent = <0x1>;
        phy-handle = <0x2>;
        #address-cells = <0x1>;
        #size-cells = <0x0>;
        xlnx,ptp-enet-clock = <0x69f6bc7>;
        xlnx,slcr-div0-1000Mbps = <0x8>;
        xlnx,slcr-div0-100Mbps = <0x8>;
        xlnx,slcr-div0-10Mbps = <0x8>;
        xlnx,slcr-div1-1000Mbps = <0x1>;
        xlnx,slcr-div1-100Mbps = <0x5>;
        xlnx,slcr-div1-10Mbps = <0x32>;

        mdio {
            #address-cells = <0x1>;
            #size-cells = <0x0>;

            phy@0 {
                compatible = "marvell,88e1510";
                device_type = "ethernet-phy";
                reg = <0x0>;
                marvell,reg-init = <0x3 0x10 0xff00 0x1e 0x3 0x11 0xfff0 0xa>;
                linux,phandle = <0x2>;
                phandle = <0x2>;
            };
        };
    };

    Please let us know if you find something useful.

    Regards,

    -Kevin

    P.S.  Sorry about the code snippet formatting, the forum editor seems to enjoy chewing these up.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 13 years ago

    Seetharam,

    I am glad that we are both seeing the same behavior even though it might not be the expected behavior.

    I don't think that there were any changes made within the Ethernet driver itself for ZedBoard.  I would suggest taking a look at the device tree entry for the Ethernet driver and see if there are any differences from the device tree entry used for ZC702. 

    This may help you isolate a chip specific setting that you might need for your BSP code.

    Here is the Ethernet device entry for ZedBoard out-of-box demos:

    eth@e000b000 {
        compatible = "xlnx,ps7-ethernet-1.00.a";
        reg = <0xe000b000 0x1000>;
        interrupts = <0x0 0x16 0x0>;
        interrupt-parent = <0x1>;
        phy-handle = <0x2>;
        #address-cells = <0x1>;
        #size-cells = <0x0>;
        xlnx,ptp-enet-clock = <0x69f6bc7>;
        xlnx,slcr-div0-1000Mbps = <0x8>;
        xlnx,slcr-div0-100Mbps = <0x8>;
        xlnx,slcr-div0-10Mbps = <0x8>;
        xlnx,slcr-div1-1000Mbps = <0x1>;
        xlnx,slcr-div1-100Mbps = <0x5>;
        xlnx,slcr-div1-10Mbps = <0x32>;

        mdio {
            #address-cells = <0x1>;
            #size-cells = <0x0>;

            phy@0 {
                compatible = "marvell,88e1510";
                device_type = "ethernet-phy";
                reg = <0x0>;
                marvell,reg-init = <0x3 0x10 0xff00 0x1e 0x3 0x11 0xfff0 0xa>;
                linux,phandle = <0x2>;
                phandle = <0x2>;
            };
        };
    };

    Please let us know if you find something useful.

    Regards,

    -Kevin

    P.S.  Sorry about the code snippet formatting, the forum editor seems to enjoy chewing these up.