Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Ethernet is not running in Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 374 subscribers
  • Views 3753 views
  • Users 0 members are here
Related

Ethernet is not running in Zedboard

e14 Contributor
e14 Contributor over 13 years ago

I was trying to migrate the WinCE BSP for Xilinx ZC702 for ZedBoard and got stuck in getting the Ethernet working.
After I change the PHY address to 0 it successfully completes the autonegotiation and reports the link speed. There after it fails and looks like it is not receiving any frames.
I blamed the PHY chip differences and spend couple of days in the data sheets and no luck. At that point I thought of trying with the supplied Linux boot image(till then I used the xilinx XPS and run the sample based on the hw definition file from Zedboard and didn't check the LAN).
Surprisingly it didn't even do the self pinging, I changed the IP address but it stuck with the ping command as follows
PING 192.168.1.10 (192.168.1.10): 56 data bytes

Out of the 3 boards we have I checked two and got the same results. Any help is much appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • zedhed
    zedhed over 13 years ago +1
    Hi Seetharam, We have a Getting Started Guide posted in the Documents section on ZedBoard.org which contains a section on using the ZedBoard Ethernet. http://zedboard.org/sites/default/files/documentations…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I've run into this issue with Xilinx Zynq-7000 AP SoC ZC706 Evaluation Kit.

    Issue:
    DHCP was working after running dhclient. The tx packet counter increases to 1, but I could not send any other packets. Receiving packets seems to work as the rx packet counter increases. It isn't a hardware problem as DHCP was working.
    I tried replacing the kernel, modified the device tree and changed kernel args, but no luck.

    Solution:
    I downloaded the prebuilt FSBL.elf from
    http://www.wiki.xilinx.com/Zynq+14.6-2013.2+Release
    and created a new boot.bin.
    Now everything works.

    For reference see here:
    http://forums.xilinx.com/t5/Xilinx-Boards-and-Kits/zc706-ethernet-does-not-work/td-p/347803

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I've run into this issue with Xilinx Zynq-7000 AP SoC ZC706 Evaluation Kit.

    Issue:
    DHCP was working after running dhclient. The tx packet counter increases to 1, but I could not send any other packets. Receiving packets seems to work as the rx packet counter increases. It isn't a hardware problem as DHCP was working.
    I tried replacing the kernel, modified the device tree and changed kernel args, but no luck.

    Solution:
    I downloaded the prebuilt FSBL.elf from
    http://www.wiki.xilinx.com/Zynq+14.6-2013.2+Release
    and created a new boot.bin.
    Now everything works.

    For reference see here:
    http://forums.xilinx.com/t5/Xilinx-Boards-and-Kits/zc706-ethernet-does-not-work/td-p/347803