Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Zedboard Clock Speed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 366 subscribers
  • Views 2261 views
  • Users 0 members are here
Related

Zedboard Clock Speed

Former Member
Former Member over 13 years ago

I have ported LMBench to run on the Zedboard, and in doing so the benchmark reported that the core is running at 800MHz, not 677MHz.  I'm running Linaro's nano linux as my OS.

I decided to dig deeper, and found that there's supposed to be a speed grade marking on the chip right before the CLG484 text.  On my chip, there is no speed grade marking.  I'm wondering if the board I have is actually an 800MHz board?

I've also heard the dev/eval kit board chips have the exact same text written on them as the Zedboard chips.

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 13 years ago

    The current ZedBoards have ES Zynq silicon, which does not have a speed grade, which would explain why you see no marking in the speed grade position.  When production Zynq silicon is available, the ZedBoard will ship with a -1 device, which has a max cpu clock frequency of 667 MHz.

     

    The default design that ships with the ZedBoard is set to 667 MHz, as is the default XML board description file.  It is possible that ZedBoards with ES silicon will operate at 800 MHz, but that is not the intention given the plans to ship with a -1.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 13 years ago

    The current ZedBoards have ES Zynq silicon, which does not have a speed grade, which would explain why you see no marking in the speed grade position.  When production Zynq silicon is available, the ZedBoard will ship with a -1 device, which has a max cpu clock frequency of 667 MHz.

     

    The default design that ships with the ZedBoard is set to 667 MHz, as is the default XML board description file.  It is possible that ZedBoards with ES silicon will operate at 800 MHz, but that is not the intention given the plans to ship with a -1.

     

    Bryan