Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General 7" zed touch display kit
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 374 subscribers
  • Views 483 views
  • Users 0 members are here
Related

7" zed touch display kit

e14 Contributor
e14 Contributor over 12 years ago

I have been trying to run the tutorial programs for the 7" zed touch display kit but I have been facing this problem where I get the following error:

ERROR : Failed to write Touch Controller

I have narrowed down the error to the point where the program attempts to send 2 bytes of data using IIC. Specifically at the final few lines of the program. I'm not sure what exactly it is writing to, I can only guess that it's writing something to the ALI3 sharp interface or the LCD interface, but I'm not sure what it is trying to trigger with the final write.

int zed_ali3_controller_demo_init( zed_ali3_controller_demo_t *pDemo )
{
   int ret;

   xil_printf("
r");
   xil_printf("------------------------------------------------------
r");
   xil_printf("--              ZedBoard Display Kit                --
r");
   xil_printf("--           ALI3 Controller Demonstration          --
r");
   xil_printf("--             Standalone Application               --
r");
   xil_printf("------------------------------------------------------
r");
   xil_printf("
r");

   // Fill frame stores with color bars
   xil_printf( "Video Frame Buffer Initialization ...
r" );
   int32u frame, row, col;
   int32u pixel;
   volatile int32u *pStorageMem = (int32u *)pDemo->uBaseAddr_MEM_FrameBuffer;
   for ( frame = 0; frame < pDemo->uNumFrames_FrameBuffer; frame++ )
   {
      for ( row = 0; row < pDemo->ali3_height; row++ )
      {
         for ( col = 0; col < pDemo->ali3_width; col++ )
         {
             pixel = 0x00000000; // Black
             //pixel = 0x00FFFFFF; // White
             *pStorageMem++ = pixel;
          }
       }
    }

    // Wait for DMA to synchronize.
    Xil_DCacheFlush();

   // Initialize Output Side of AXI VDMA
   xil_printf( "Video DMA (Output Side) Initialization ...
r" );
   vfb_common_init(
      pDemo->uDeviceId_VDMA_FrameBuffer, // uDeviceId
      &(pDemo->vdma_ali3)                // pAxiVdma
      );
   vfb_tx_init(
      &(pDemo->vdma_ali3),               // pAxiVdma
      &(pDemo->vdmacfg_ali3_read),       // pReadCfg
      pDemo->ali3_resolution,            // uVideoResolution
      pDemo->ali3_resolution,            // uStorageResolution
      pDemo->uBaseAddr_MEM_FrameBuffer,  // uMemAddr
      pDemo->uNumFrames_FrameBuffer      // uNumFrames
      );

   // IIC Initialization for touch controller
   xil_printf( "I2C Touch Controller Initialization ...
r");
   ret = zed_iic_axi_init(&(pDemo->touch_iic),"ALI3 Touch I2C Controller0", pDemo->uBaseAddr_IIC_Touch);
   if ( !ret )
   {
      xil_printf("ERROR : Failed to open ZED-IIC driver
r");
      return -1;
   }

   pDemo->touch_irqs   = 0;
   pDemo->touch_events = 0;
   pDemo->touch_posx   = 0x0000;
   pDemo->touch_posy   = 0x0000;

   zed_ali3_controller_demo_SetupInterruptSystem( pDemo );


      int8u ChipAddress = 0x20;
      int8u RegAddress  = 0x00;
      int8u RegData     = 0x11; // [4] = INT enabled, [0] = Touch enabled
      int8u ByteCount   = 1;
      ret = pDemo->touch_iic.fpIicWrite( &(pDemo->touch_iic), ChipAddress, RegAddress, &RegData, ByteCount );
      if ( !ret )
      {
          xil_printf( "ERROR : Failed to write Touch Controller
r" );
          return -1;
      }


   return 0;

}

Any help would be appreciated thanks =)

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    No, it was not resolved. Wasn't Kevin's fault though as I did not have the time to go through the problem with him and I made use of the screen as-is to complete whatever I needed to do. Was on a time sensitive project and actually all they ever wanted was just a screen to display what they want to see.

    Hopefully you'll get it working with Kevin. Good luck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    No, it was not resolved. Wasn't Kevin's fault though as I did not have the time to go through the problem with him and I made use of the screen as-is to complete whatever I needed to do. Was on a time sensitive project and actually all they ever wanted was just a screen to display what they want to see.

    Hopefully you'll get it working with Kevin. Good luck