Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General mpu6050(i2c based)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Subscribers 376 subscribers
  • Views 1551 views
  • Users 0 members are here
Related

mpu6050(i2c based)

473srikanth
473srikanth over 10 years ago

Hi friends,

                 i want to establish i2c communication between zedboard(ps section) and mpu6050 sensor(accelero+gyro).

                In the SDK , i'm opening iic examples. But i can open iicps examples only. Can anyone tell me , how to open iic examples instead of iicps examples ?

These examples(iicps) can help me address external devices...

               In the drivers folder of sdk, we have examples for iic and iicps.

Thanks in advance... 

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 10 years ago

    Hi 473srikanth,

    If you open the folder "C:XilinxSDK2016.2dataembeddedswXilinxProcessorIPLibdriversiic_v3_2examples" in Windows Explorer you will find a bunch of example .c files.

    Each one of those files is an example application for the IIC IP since they each contain their own main() function.  To use one of those examples, I would create a new blank application (and BSP) in SDK then drag the source file for the example you want into the "src" folder of your new blank SDK application.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 473srikanth
    0 473srikanth over 10 years ago in reply to zedhed

    Thanks a lot for the reply sir.

    I did the same thing in Linux(ubuntu). But the header files are not resolved(showing errors in #include line).

    And each header file is internally including other header files.

    Help me in resolving the headerfiles.... 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 10 years ago

    Hi 473srikanth,

    Please help me try to understand a little better what it is you are trying to do.

    You have Xilinx SDK installed under Ubuntu Linux and you are having problems creating a new blank application and adding the example code to the src/ folder of the new project?

    What are the error messages that you are seeing?  Which header files are not being resolved.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • 473srikanth
    0 473srikanth over 10 years ago in reply to zedhed

    Hi Kevin sir,

    I have Xilinx SDK installed under Ubuntu Linux. i created a blank application and copied the iic example code into src folder of my project. when i tried to build project, the following errors occured .

    fatal errors: xiic.h and xintc.h files not found.

    i found that These header files futher contains(includes/needs) other header files.    

    How can i resolve this problem of headerfiles?

    Thanks in advance ......

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gayathrivlsi
    0 gayathrivlsi over 9 years ago

    I am also getting the same error in this line:

    #include "xiic.h"

    please anyone help me to resolve the problem as soon as possible

    Thanks in advance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 473srikanth
    0 473srikanth over 9 years ago in reply to gayathrivlsi

    Hello Gayathrivlsi,

                                     Include the iic while configuring the zync processor and then generate the bit file and then export the hardware to SDK. After that,  You can use  xiicps.h header in the SDK programming.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gayathrivlsi
    0 gayathrivlsi over 9 years ago

    image

    Hai srikanth sir,

                        Fatal error is cleared . when I  try to dump my code into ZED board.  I got the internal error.

    Help me out to solve the problem.

    Thanks in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gayathrivlsi
    0 gayathrivlsi over 9 years ago

    I have to establish a i2c communication  between Accelerometer (1TG MPU 6050) and ZED board. I am using vivado 2014.1. I got the error in my design. Can anyone tell  or send me the correct block design in vivado using IP integrator ?

    please help me to resolve the problem as soon as possible.

    Thanks in advance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Gayathrivlsi,

    For educational support, I am going to suggest you use the Digilent forum.

    https://forum.digilentinc.com/

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gayathrivlsi
    0 gayathrivlsi over 9 years ago

    I have created a project in vivado and I have export to SDK. now i dont know the hardware pin configuration .

    Can anyone tell  how to connect accelerometer to the Zedboard using pmod?

    Please help me to this hardware connection.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>