Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General SD Card Fails to Boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 373 subscribers
  • Views 371 views
  • Users 0 members are here
Related

SD Card Fails to Boot

e14 Contributor
e14 Contributor over 13 years ago

Hi

The BOOT.bin on my SD Card (shipped with the board) will not run.  It has booted correctly in the past, and I have tried using the default image from the OOB design.  I tried formatting the card using mkdosfs and fdisk to see if that would fix the problem but it still won't boot.  Does anyone know if there is a specific method I need to follow to correctly format the card so it will work?

Thanks
Matthew

  • Sign in to reply
  • Cancel
  • shakith
    0 shakith over 13 years ago

    are they primary partitions? I had the same problem, when didn't set them as primary partitions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 13 years ago

    Hi m.russell,

    Once I corrupted my SD card while un-safely powering off ZedBoard while during some heavy write load to the SD card.

    Take a look at this page if you need the SD card files for the OOB demo.

    http://www.zedboard.org/node/241

    Formatting the SD card under Windows seems to work just fine on my 4GB card.  Use Windows Explorer, right click on the SD card drive and select 'Format' option.

    I was able to get away with using the defaults on Windows 7 but I usually shy away from the quick format option, just to be safe.

    Regards,

    -Kevin