Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General MicroZed Boot Problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 373 subscribers
  • Views 1038 views
  • Users 0 members are here
Related

MicroZed Boot Problem

e14 Contributor
e14 Contributor over 11 years ago

Hello All,

I have been running my MicroZed (BD-Z7MB-7Z010-G REVF06) with a Breakout Carrier Card for several months now with no issues.  Recently, however, when I booted up in SD Card mode (as per usual, I have Ubuntu loaded on there) the board & card powered up but I was unable to connect to the serial port using my terminal program.  I then tried booting up in QSPI mode and JTAG mode (which seemed to work fine, although oddly the blue "ready" light was on immediately) but I was not able to connect to either the serial port or the JTAG cable.

To isolate the problem I separated the MicroZed from the Breakout Carrier Card, and tried booting it up as a standalone device.  The MicroZed would not boot up at all when powered only by the USB cable.  I tried switching USB cables and using different USB ports, but none of the LEDs would light up.

Any troubleshooting ideas out there?

Thanks.

Adam

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 11 years ago

    Are you using a cost-optimized MicroZed? That would explain why it doesn't power up standalone?

     

    Which JTAG cable are you using? The error you listed seems to implicate the JTAG cable itself.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bhfletcher

    Gary,
    I bought the MicroZed (Evaluation Kit) and Breakout Carrier Card separately from Avnet.  I'm fairly certain that when it first arrived, I powered up the MicroZed as a standalone device to test it out.  How would I know if it is a "cost-optimized" version?  Is that indicated anywhere on the device?
    As for the JTAG cable, I bought the recommended HS2 JTAG cable (with the little adapter) directly from Digilent.
    Thanks for trying to help probe this issue.
    Adam
    P.S. Since you mention "the error you listed" I assume you were able to see my reply to Gary above.  That reply is not visible to me for some reason, even though I posted it!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bhfletcher

    Gary,
    I bought the MicroZed (Evaluation Kit) and Breakout Carrier Card separately from Avnet.  I'm fairly certain that when it first arrived, I powered up the MicroZed as a standalone device to test it out.  How would I know if it is a "cost-optimized" version?  Is that indicated anywhere on the device?
    As for the JTAG cable, I bought the recommended HS2 JTAG cable (with the little adapter) directly from Digilent.
    Thanks for trying to help probe this issue.
    Adam
    P.S. Since you mention "the error you listed" I assume you were able to see my reply to Gary above.  That reply is not visible to me for some reason, even though I posted it!