Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General MicroZed Boot Problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 373 subscribers
  • Views 1040 views
  • Users 0 members are here
Related

MicroZed Boot Problem

e14 Contributor
e14 Contributor over 11 years ago

Hello All,

I have been running my MicroZed (BD-Z7MB-7Z010-G REVF06) with a Breakout Carrier Card for several months now with no issues.  Recently, however, when I booted up in SD Card mode (as per usual, I have Ubuntu loaded on there) the board & card powered up but I was unable to connect to the serial port using my terminal program.  I then tried booting up in QSPI mode and JTAG mode (which seemed to work fine, although oddly the blue "ready" light was on immediately) but I was not able to connect to either the serial port or the JTAG cable.

To isolate the problem I separated the MicroZed from the Breakout Carrier Card, and tried booting it up as a standalone device.  The MicroZed would not boot up at all when powered only by the USB cable.  I tried switching USB cables and using different USB ports, but none of the LEDs would light up.

Any troubleshooting ideas out there?

Thanks.

Adam

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Adam,

     

    It does sound as if your board is broken.

     

    I don't think the 10 week lead time is accurate. I believe we will have MicroZed boards pretty soon but I will check and post the expected availability when I can confirm a date.


    The Cost Optimized MicroZed SOM which, like the MicroZed SOM, comes in the four versions and has no cables, voucher or microSD card. This version costs a little less and is intended for production where the customer is going to operate only in a carrier card environment where power is supplied by the carrier card as well as the JTAG connections. The boot options are fixed as well as a couple of other changes such as no user LED and push button. AES-Z7MB-7Z0x0-C01-x-G 
    This post has additional details on the Cost Optimized MicroZed:
     http://zedboard.org/content/what-cost-optimized-c01-microzed-som

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Adam,

     

    It does sound as if your board is broken.

     

    I don't think the 10 week lead time is accurate. I believe we will have MicroZed boards pretty soon but I will check and post the expected availability when I can confirm a date.


    The Cost Optimized MicroZed SOM which, like the MicroZed SOM, comes in the four versions and has no cables, voucher or microSD card. This version costs a little less and is intended for production where the customer is going to operate only in a carrier card environment where power is supplied by the carrier card as well as the JTAG connections. The boot options are fixed as well as a couple of other changes such as no user LED and push button. AES-Z7MB-7Z0x0-C01-x-G 
    This post has additional details on the Cost Optimized MicroZed:
     http://zedboard.org/content/what-cost-optimized-c01-microzed-som

     

    -Gary