Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Zedboard and ARM DS-5
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 373 subscribers
  • Views 779 views
  • Users 0 members are here
Related

Zedboard and ARM DS-5

e14 Contributor
e14 Contributor over 13 years ago

Hi everybody,

I program bare-metal applications on the Zedboard with the Xilinx SDK. But now, I wanted to program the ARM processor on the Zedboard out of the ARM Development Suite 5.
But I don't find any information, how I can program the processor on the Zedboard out of ARM DS-5 over the Onboard USB-JTAG adapter.

If anyone of you has any experience with that, it would be glad if he could help me, or give me a hint, how I can do this.

Best regards
Jan

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 13 years ago

    Hi Jan,

    Just to follow up on this, for those of you trying to create your own adapter, some ARM debugger tools require the ability to 'see' the processor come out of reset. 

    To do this, tools will monitor the state of processor reset and so a connection is required between pin 15 (nRST) of the 20-pin ARM cable and pin 14 (PROG-RST) of ZedBoard J15 is required.  Also, be sure to place a jumper at JP13 so that PROG-RST is connected to the Zynq PS-RST input.

    Having the reset connected also allows the debugger tools to reset the processor via PS-RST instead of doing this through the JTAG chain.

    As for the remainder of the connections, one thing to keep in mind to check is the TDI to TDI and TDO to TDO as some 3rd party tools tend to cross these signals for some reason.  One sure fire method is to simply map the pin numbers from the ARM 20-pin cable format to the Xilinx 14-pin PC4 cable format.  Here is the map from 20-pin connector to 14-pin connector that we use which works with the ARM DSTREAM.
     
    1)  ARM pin 1 tied directly to 3.3V which is available as ZedBoard J15 pin 2.
    2)  ARM 4,6,8,10,12,14,16,18,20 tied directly to GND which is available on ZedBoard J15 pins 1,3,5,7,9,11,13.
    3)  ARM pin 5 is connected to the same ZedBoard signal as J15 pin 10.
    4)  ARM pin 7 is connected to the same ZedBoard signal as J15 pin 4.
    5)  ARM pin 9 is connected to the same ZedBoard signal as J15 pin 6.
    6)  ARM pin 13 is connected to the same ZedBoard signal as J15 pin 8.

    You should be able to get the same information from the adapter schematic but I just noticed that the schematic has not been posted to our DRC yet.  I will look into this, it should get posted in just a few more days.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 13 years ago in reply to zedhed

    As an update to this, it looks like the schematics, PCB artwork, and BOM documents are now posted on our Design Resource Center under the "Support Files & Downloads" link of the ZedBoard Processor Debug Adapter product page found here:

    http://www.em.avnet.com/zeddebugadapter

    We are working on some tutorial material that will be posted in the near future so stay tuned...

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 13 years ago in reply to zedhed

    As an update to this, it looks like the schematics, PCB artwork, and BOM documents are now posted on our Design Resource Center under the "Support Files & Downloads" link of the ZedBoard Processor Debug Adapter product page found here:

    http://www.em.avnet.com/zeddebugadapter

    We are working on some tutorial material that will be posted in the near future so stay tuned...

    Regards,

    -Kevin