Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Add driver to linux kernel
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 372 subscribers
  • Views 951 views
  • Users 0 members are here
Related

Add driver to linux kernel

e14 Contributor
e14 Contributor over 9 years ago

Hi,

I need to transfer video data into DDR and read it back. I want to add the VDMA driver from Xilinx-github

(https://github.com/Xilinx/linux-xlnx/blob/master/drivers/dma/xilinx/xilinx_dma.c)

I've tried the instructions in the ReadMe file but unable to compile it.

How can I build the kernel using it ?

Also do I need PetaLinux for this purpose  ?

 

Thanks in Advance

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 9 years ago +1 verified
    Downloaded kernel from https://github.com/Digilent/linux-digilent error would be regarding "awk" so follow http://www.googoolia.com/wp/2015/04/21/awk-symbol-lookup-error-awk-undefined-symbol-mpfr_z_sub…
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Downloaded kernel from  https://github.com/Digilent/linux-digilent

    error would be regarding "awk" so follow  http://www.googoolia.com/wp/2015/04/21/awk-symbol-lookup-error-awk-undefined-symbol-mpfr_z_sub/ 

    and modify file .settings64.sh

    If using a 64bit OS then install 32bit packages  

    sudo apt-get install gawk

    sudo apt-get install build-essential

    sudo apt-get install automake

    sudo apt-get install libtool

    sudo apt-get install lib32ncurses5

    sudo apt-get install lib32ncurses5-dev

    sudo apt-get install lib32ncursesw5

    sudo apt-get install ncurses-dev:i386

    sudo apt-get install libstdc++6:i386

    sudo apt-get install libselinux1:i386

     


    (from http://blog.idv-tech.com/2014/02/19/update-u-boot-and-linux-kernel-for-petalinux-13-10/)

    now open a new terminal from the extracted files downloaded for kernel from github and type

     

    export CROSS_COMPILE=arm-xilinx-linux-gnueabi-

    source /Xilinx/SDK/2015.2/settings64.sh   (path to SDK source file)

     

    follow http://www.wiki.xilinx.com/Build+Kernel

    finally built kernel will be at   /path/to/linux-digilent-master-main/arch/arm/boot

     

    Hope this can be useful to others

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer