Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Cypress Driver and Windows 7
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 373 subscribers
  • Views 282 views
  • Users 0 members are here
Related

Cypress Driver and Windows 7

e14 Contributor
e14 Contributor over 11 years ago

This is probably a Cypress USB-UART question (more so than Zedboard), but I am wondering if anyone else has had issues with the USB UART driver hanging on port opening (from the PC side)?

I have used the Zedboard USB UART 1000s of times as an A9 menu system on both a WinXP and Win7 (Home) machine, but am now trying to use it on new Win7 Professional machine, and the port will hang on the attempt to open the port.

This happens on both an open of Putty (in serial mode), and in a Win32 console program on a CreateFile call, which is the first step in opening a COM port.

On the Win7 Pro machine, I have found that after launching Putty, it will hang.  However, if I then power-cycle the Zedboard, the Putty terminal window will appear, and the USB UART terminal session will operate normally thereafter.

According to device manager, both of my Win7 x64 machines have the same drivers loaded.  (Loaded per the instructions on v1.3 of the Zedboard USB-UART app note).

I am stumped, and am curious if anyone else has seen odd behavior with opening the USB UART port on Zedboard, particularly in a Win7 Pro environment.  Thanks!

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Do you have the latest Cypress driver? I checked and on two Win7 Pro machines the Cypress driver is version 3.13.0.32, dated 8/12/2014.

     

    The driver is working fine on both machines.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thank you for the confirmation on Win 7 Pro working fine.  Unfortunately, that is the driver version that my Win 7 PCs are using, so it does not look like an easy driver fix.