Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Petalinux interface with Custom IP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 372 subscribers
  • Views 566 views
  • Users 0 members are here
Related

Petalinux interface with Custom IP

e14 Contributor
e14 Contributor over 10 years ago

I am quite new in this,,in Petalinux I would like to control a custom IP (device) via using the the memory space dev/mem to send or receive a value of 32 bit

I have seen some examples but I have a bit struggle in understanding the following values in the examples , and how to identify them


Page size
Page adress
Page offset
Adress

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Oggo,

    To work with linux drivers, you will need to have a good understanding of the difference between kernel space and user space.  Application programs run in virtual memory, which is a mechanism designed to make applications think they have access to the entire physical memory when really they are separated from each other by the operating system.  This prevents programs from interacting with each other.  In kernel space, there are no such safeguards, so you need to understand how the memory controller works and how memory is mapped at a more fundamental level, and all of the terms you list apply here.

    If you truly want to understand this area, I'd recommend that you locate some reference material on the Linux kernel, and read through the relevent chapters.  For example, there is a series of text from O'Reilly that does an excellent job of describing kernel operations.  You might want to start with "Understanding the Linux Kernel".  There are also innumerable online references to the terms you ask about, but it is often difficult to put the information in context without a suitable grounding the in the material.

    It's a very interesting area for developers, and I wish you well in your studies.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hey Ron

     

         Thanks for the answer and the recommendations  , I ll give it a try :)