Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General how to modify run level in zed board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 374 subscribers
  • Views 957 views
  • Users 0 members are here
Related

how to modify run level in zed board

e14 Contributor
e14 Contributor over 11 years ago

hi,

can you give the suggestion how to modify the run level in zed board. i tried to modify the run level in /etc/inittab file id:1:initdefault instead of id:5:initdefault: .but it is not changed. so anyone have an idea regarding this issue. please suggest me and how to remove the login id and password after booting the zed board.



Thanks & Regards,
srinivas Rao

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    Hi Srinivas,

    Okay, I think I see what you are doing.

    What I am getting at is that you should be able to modify your RAM disk image (in your case it is the rootfs.cpio file) from your PetaLinux development machine.

    Here are the steps that I used to unpack, modify, and repack one on my development system:

    1)  Create a temporary folder to hold your root file system so that it can be unpacked in the next step:

    mkdir tmp_mnt

    2)  Unpack the cpio archive to the temporary folder:

    cd tmp_mnt/
    sudo cpio -i < ../rootfs.cpio

    3)  Make the desired modifications to the root file system files (in this step I did my edits to tmp_mnt/etc/inittab and created the autologin.sh script in tmp_mnt/home/root/).

    4)  Once the modifications are complete, repack the cpio archive (starting from the tmp_mnt/ working directory):

    cd ..
    rm rootfs.cpio
    sh -c 'cd tmp_mnt/ && sudo find . | sudo cpio -H newc -o' > rootfs.cpio

    Now copy the updated rootfs.cpio image to your SD card and boot ZedBoard, you should see the modifications to the root file system in place at this point.

    The bottom line is that yes you are correct in that any changes you make to the file system while it is loaded into RAM on ZedBoard will not persist between reboots.  However, you should be able to modify that file system image on your development machine to suit your needs.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 11 years ago

    Hi Srinivas,

    Okay, I think I see what you are doing.

    What I am getting at is that you should be able to modify your RAM disk image (in your case it is the rootfs.cpio file) from your PetaLinux development machine.

    Here are the steps that I used to unpack, modify, and repack one on my development system:

    1)  Create a temporary folder to hold your root file system so that it can be unpacked in the next step:

    mkdir tmp_mnt

    2)  Unpack the cpio archive to the temporary folder:

    cd tmp_mnt/
    sudo cpio -i < ../rootfs.cpio

    3)  Make the desired modifications to the root file system files (in this step I did my edits to tmp_mnt/etc/inittab and created the autologin.sh script in tmp_mnt/home/root/).

    4)  Once the modifications are complete, repack the cpio archive (starting from the tmp_mnt/ working directory):

    cd ..
    rm rootfs.cpio
    sh -c 'cd tmp_mnt/ && sudo find . | sudo cpio -H newc -o' > rootfs.cpio

    Now copy the updated rootfs.cpio image to your SD card and boot ZedBoard, you should see the modifications to the root file system in place at this point.

    The bottom line is that yes you are correct in that any changes you make to the file system while it is loaded into RAM on ZedBoard will not persist between reboots.  However, you should be able to modify that file system image on your development machine to suit your needs.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to zedhed

    Hi kevin,


    i have done as per previous information.

    root@pradeep-desktop:/home/pradeep~#mkdir rootfs
    root@pradeep-desktop:~#cd rootfs/
    root@pradeep-desktop:/home/pradeep/rootfs#

    i copied rootfs.cpio gile in this folder

    root@pradeep-desktop:/home/pradeep/rootfs~#cpio -i < rootfs.cpio

    root@pradeep-desktop:/home/pradeep/rootfs~#vim /home/root/autologin.sh

    #!/bin/sh
    exec /bin/login -f root

    root@pradeep-desktop:/home/pradeep/rootfs/home/root~#chmod a+x autologin.sh

    Modified my /etc/inittab file

    #PS0:2345:respawn:/sbin/getty -L 115200 ttyPS0 vt100
    PS0:2345:respawn:/sbin/getty -l /home/root/autologin.sh -n -L 115200 ttyPS0 vt100

    root@pradeep-desktop:/home/pradeep/rootfs~#rm rootfs.cpio

    root@pradeep-desktop:/home/pradeep/rootfs~#cd ..
    root@pradeep-desktop:/home/pradeep~#sh -c 'cd rootfs/ && sudo find . | sudo cpio -H newc -o' > rootfs.cpio


    everything clear upto this


    these are  mtd parititions

    0x000000000000-0x000000500000 : "boot"
    0x000000500000-0x000000520000 : "bootenv"
    0x000000520000-0x000000fa0000 : "kernel"
    0x000000fa0000-0x000002000000 : "spare"

    //............................... mtd3 partition...........................................//

    flash_eraseall -j /dev/mtd3
    flashcp -v  rootfs.cpio /dev/mtd3

    //.........................my uboot commands...............................................//

    bootargs=console=ttyPS0,115200 root=/dev/mtd3 rw earlyprintk 5
    qspiboot_test=sf probe 0 0; sf read 0xfa0000 0x520000 0xa80000 && sf read 0x2000000 0xfa0000 0x1060000 && bootm 0xfa0000 0x2000000

    //..........i am getting like this ....................................//

    U-Boot-PetaLinux> run qspiboot_test
    SF: Detected S25FL256S_64K with page size 256 Bytes, erase size 64 KiB, total 32 MiB
    SF: 11010048 bytes @ 0x520000 Read: OK
    SF: 17170432 bytes @ 0xfa0000 Read: OK
    ## Loading kernel from FIT Image at 00fa0000 ...
       Using 'conf@1' configuration
       Trying 'kernel@1' kernel subimage
         Description:  PetaLinux Kernel
         Type:         Kernel Image
         Compression:  gzip compressed
         Data Start:   0x00fa00f0
         Data Size:    7150584 Bytes = 6.8 MiB
         Architecture: ARM
         OS:           Linux
         Load Address: 0x00008000
         Entry Point:  0x00008000
         Hash algo:    crc32
         Hash value:   5d7f745d
       Verifying Hash Integrity ... crc32+ OK
    Wrong Ramdisk Image Format
    Ramdisk image is corrupt or invalid
    U-Boot-PetaLinux>


    can you tell me  where i did the mistake.


    Thanks & Regards,
    srinivas Rao