Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General File io program - Zed board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 372 subscribers
  • Views 379 views
  • Users 0 members are here
Related

File io program - Zed board

e14 Contributor
e14 Contributor over 9 years ago

I have a problem in creating FILE pointer like FILE *fp; and then i opend a file like fp = fopen("c:/user/xilinx/project1/hello.txt","w");
and I didn't get any address in file pointer while debugging and i didn't get any dump file hello.text in my project1,, help me

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Viswapraveen

    Assuming that you are attempting to program a Zynq device on something like a Zedboard, you need to first understand the embedded system you are working with. Programming on the Zynq is not the same as writing a C program to run under Windows on your PC. The statement you have listed above assumes that there is a "C:" hard drive available to the system (C: is on your host PC, not on the ZedBoard), and that you have a file system implemented on the "C" drive, and that you have an operating system, like Windows, that  supports the 'fopen' operation.
     
    On a ZedBoard there is only the RAM memory internal to the Zynq device, the DDR3 DRAM, the SD Card (if installed) and the QSPI Flash device, no 'C' hard drive. Then, to perform a file operation on one of these available memory resources, you would need to implement an Operating System (such as Linux, PetaLinux, FreeRTOS, etc.) or at least one of the file system libraries (xilmfs).
     
    I suggest that you study to familiarize yourself with the Zynq system by using the resources referred to the answer in this posts: http://www.zedboard.org/content/helloworldelf-storage-location-zedboard
     
    Then perhaps move on to the PetaLinux Speedway material available at the same page pointed to for the Zynq Software and Hardware Speedway material or some other resources for embedded systems.
     
    --Josh