Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General MicroZed - Ethernet Issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 374 subscribers
  • Views 586 views
  • Users 0 members are here
Related

MicroZed - Ethernet Issue

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I have two Microzed board. The first own a 7010 Zynq and the second a 7020 Zynq. My goal is to download/debug an application over TCP/IP. The Zynqs are configured with the default linux on QSPI Flash

My computer has the following IP : 10.0.10.73 and Mask : 255.255.254.0

To ping my 7010 board from my computer I have changed the ip of the Zynq as follow : ifconfig eth0 10.0.10.100. It works fine, but when I do the same with the 7020 it doesn't work at all. The Leds on the RJ45 are blinking continously and when I ping from my computer nothing happen.

Can someone help me ??

Thanks..

Regards,

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 12 years ago

    Hi Snoopy_87,

    I tested this on my end with my 7020 MicroZed and I am able to ping it successfully.

    This is how I have my test network setup which is similar to what is used at the factory when these modules are tested:

    Windows 7 PC: 192.168.1.100
    MicroZed 7020: 192.168.1.10

    Occasionally, something in the networking configuration gets messed up and requires the eth0 to be restarted.  Have you tried bringing down the eth0 interface and bringing it back up to a known good state:

    ifconfig eth0 down
    ifconfig eth0 up

    Also, when you are changing the IP address on MicroZed, are you assigning it a compatible netmask to the IP address scheme for your network?  In the Out Of Box Linux within QSPI, MicroZed is configured for the following:

    inet: 192.168.1.10
    mask: 255.255.255.0

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    Thanks for the response. I have solved my issue. I just need to restart the eth0 and it works fine.

    Thanks,

    Regards