Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General u-boot hangs immediately on new 04/2014 Rev D boards
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 372 subscribers
  • Views 662 views
  • Users 0 members are here
Related

u-boot hangs immediately on new 04/2014 Rev D boards

vadimv
vadimv over 12 years ago

Hello,

I have a Zynq PS/PL design that happily runs on my two Rev D Zedboards, boots using tftpboot, runs great. I'm a longtime Zedboard/Xilinx user, never had serious problems before.

I recently bought 8 new Rev D boards to share with the rest of my development team. I have tried all 8 - every single one fails to boot in the exact same setup as my original 2 that work. I power off working board, unplug, plug in new board exactly the same way, and fail. Booting from JTAG, u-boot gets to approx this step and hangs:

I2C:   ready
Memory: ECC disabled
DRAM: 

Sometimes it hangs when printing out the Memory: line, sometimes in the following line. I can turn off and unplug new Rev D, plug in old Red D, power on, and boot like a champ, so nothing is really changing... The truly bizzare thing is that this behavior only happens on JTAG/TFTP boot. SD card boot works fine. There's nothing in my network for controlling MAC addresses, all the boards look the same to the network. Nonetheless, u-boot fails to load way before  the TFTP step.

New boards have an 0814 datecode and S/N of D57XXXX. Additionally, the new boards have different markings on the DDR3 chips - 4CK77 D9PTK. Old Rev Ds that work were 1334 datecode and had DDR3 of 2WD22 D9LGQ, with an S/N of D53XXXX. That's the only difference, these boards are the same rev after all...

Anyone know what could be happening?  

  • Sign in to reply
  • Cancel
Parents
  • vadimv
    0 vadimv over 12 years ago

    Yes, the flow and use case for the ps7_init files is well understood... "My Hardware" is referring to ps7_init files generated when the platform is exported from Vivado. "ZED Hardware" is when one goes into SDK and creates a platform+BSP targeting the canned (pre-defined) ZED board design.


    I have failures in both cases, so the easiest way to duplicate my setup is to create the basic ZED board BSP in SDK from the pre-defined HW Platform, and use that as the configuration for export to PetaLinux. I have no particular kernel configs that are unique, so there really shouldn't be much to modify, but turn on SD as a boot source, which shouldn;t matter in the JTAG case. Doing this I rarely even get u-boot running. Need to get in there with the debugger and see what's going on.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vadimv
    0 vadimv over 12 years ago

    Yes, the flow and use case for the ps7_init files is well understood... "My Hardware" is referring to ps7_init files generated when the platform is exported from Vivado. "ZED Hardware" is when one goes into SDK and creates a platform+BSP targeting the canned (pre-defined) ZED board design.


    I have failures in both cases, so the easiest way to duplicate my setup is to create the basic ZED board BSP in SDK from the pre-defined HW Platform, and use that as the configuration for export to PetaLinux. I have no particular kernel configs that are unique, so there really shouldn't be much to modify, but turn on SD as a boot source, which shouldn;t matter in the JTAG case. Doing this I rarely even get u-boot running. Need to get in there with the debugger and see what's going on.