Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General USB Mouse not mount
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 373 subscribers
  • Views 456 views
  • Users 0 members are here
Related

USB Mouse not mount

e14 Contributor
e14 Contributor over 11 years ago

Hi,



I just finished to build all files for boot Linux (Linaro) on my Zedboard. When Linaro is booting up the USB mouse is not mount. I have this message :
ALSA device list:
  #0: HDMI monitor
  #1: ZED ADAU1761
EXT4-fs (mmcblk0p2): warning: mounting fs with errors, running e2fsck is recommended
EXT4-fs (mmcblk0p2): Errors on filesystem, clearing orphan list.
EXT4-fs (mmcblk0p2): recovery complete
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.


I should have :


ALSA device list:
  #0: HDMI monitor
  #1: ZED ADAU1761
input: DELL DELL USB Laser Mouse as /devices/amba.1/e0002000.usb/zynq-ehci.0/usb1/1-1/u200B1-1:1.0/input/input0
hid-generic 0003:046D:C063.0001: input,hidraw0: USB HID v1.10 Mouse [DELL DELL USB Laser Mouse] on usb-zynq-ehci.0-1/input0
random: nonblocking pool is initialized
EXT4-fs (mmcblk0p2): 2 orphan inodes deleted
EXT4-fs (mmcblk0p2): recovery complete
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.




Thanks

Jo

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Jo,

      Is this repeatable?  I've seen these types of errors on occasion, but generally if you restart from power-up, it works.  I'm speculating here, but I've seen this type of behavior when some transient error occupies the CPU and another process (USB device init in this case) times out and never gets set up correctly.  You can also try unplugging and re-plugging the mouse to a different USB port on the board to see if it gets picked up.  Is the keyboard working correctly, or are all USB devices unavailable?

    In this case it looks like the transient error is a problem with the file system.   Note that since the file system is persistent on the microSD partition, when you shut down the Linux desktop you should take care to shutdown correctly and not simply power off the board.   That can cause inconsistencies in the persistent file system due to writes being interrupted before they are completed.  If you can't get the USB to work at all, something you can try is to reinstall the file system from the Linaro image to the ext4 partition.

    Power down the Ubuntu system by shutting it down from the desktop as you would a real PC system, or use the shutdown now -h command from the root console.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Jo,

      Is this repeatable?  I've seen these types of errors on occasion, but generally if you restart from power-up, it works.  I'm speculating here, but I've seen this type of behavior when some transient error occupies the CPU and another process (USB device init in this case) times out and never gets set up correctly.  You can also try unplugging and re-plugging the mouse to a different USB port on the board to see if it gets picked up.  Is the keyboard working correctly, or are all USB devices unavailable?

    In this case it looks like the transient error is a problem with the file system.   Note that since the file system is persistent on the microSD partition, when you shut down the Linux desktop you should take care to shutdown correctly and not simply power off the board.   That can cause inconsistencies in the persistent file system due to writes being interrupted before they are completed.  If you can't get the USB to work at all, something you can try is to reinstall the file system from the Linaro image to the ext4 partition.

    Power down the Ubuntu system by shutting it down from the desktop as you would a real PC system, or use the shutdown now -h command from the root console.

    Ron