Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General USB Mouse not mount
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 373 subscribers
  • Views 454 views
  • Users 0 members are here
Related

USB Mouse not mount

e14 Contributor
e14 Contributor over 11 years ago

Hi,



I just finished to build all files for boot Linux (Linaro) on my Zedboard. When Linaro is booting up the USB mouse is not mount. I have this message :
ALSA device list:
  #0: HDMI monitor
  #1: ZED ADAU1761
EXT4-fs (mmcblk0p2): warning: mounting fs with errors, running e2fsck is recommended
EXT4-fs (mmcblk0p2): Errors on filesystem, clearing orphan list.
EXT4-fs (mmcblk0p2): recovery complete
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.


I should have :


ALSA device list:
  #0: HDMI monitor
  #1: ZED ADAU1761
input: DELL DELL USB Laser Mouse as /devices/amba.1/e0002000.usb/zynq-ehci.0/usb1/1-1/u200B1-1:1.0/input/input0
hid-generic 0003:046D:C063.0001: input,hidraw0: USB HID v1.10 Mouse [DELL DELL USB Laser Mouse] on usb-zynq-ehci.0-1/input0
random: nonblocking pool is initialized
EXT4-fs (mmcblk0p2): 2 orphan inodes deleted
EXT4-fs (mmcblk0p2): recovery complete
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.




Thanks

Jo

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Problem solved.
    In the .dts file I added : dr_mode="host" (in the USB node) in order to put the USB in host mode.
    Jo

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Problem solved.
    In the .dts file I added : dr_mode="host" (in the USB node) in order to put the USB in host mode.
    Jo