Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Bootgen vs mkimage with U-Boot SPL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 373 subscribers
  • Views 3612 views
  • Users 0 members are here
Related

Bootgen vs mkimage with U-Boot SPL

e14 Contributor
e14 Contributor over 10 years ago
I have created a U-Boot bootloader and Linux operating system using Buildroot
 
    git clone git://git.buildroot.net/buildroot
    cd buildroot
    make zynq_zed_defconfig
    make
 
This was successful, and I am able to boot Linux on my ZedBoard using a microSD as the boot device and using the BOOT.BIN that buildroot/U-Boot created from the U-Boot SPL binary.
 
The latest buildroot version uses U-Boot's mkimage to create a Zynq-compatible first stage bootloader from the U-Boot SPL binary (u-boot-spl.bin). I think this used to require a special python tool, but now mkimage has been given the ability to generate this binary itself.
 
However, I would like to experiment with the Xilinx bootgen tool instead of mkimage. Unfortunately, when I use bootgen, the resulting BOOT.BIN does not work.
 
I am using a BIF file (boot.bif) as follows:
 
    image:
    {
        [bootloader] u-boot-spl.bin
    }
 
I am invoking bootgen like this:
 
    bootgen -arch zynq -image boot.bif -o BOOT.BIN
 
The resulting BOOT.BIN file is 90600 bytes, which is larger than what I create using mkimage (86952 bytes):
 
    $ mkimage -A arm -T zynqimage -d u-boot-spl.bin BOOT.BIN
    Image Type   : Xilinx Zynq Boot Image support
    Image Offset : 0x000008c0
    Image Size   : 86952 bytes (86952 bytes packed)
    Image Load   : 0x00000000
    User Field   : 0x00000000
    Checksum     : 0xfd17ac31
 
Can anyone tell me how to get bootgen to generate a bootable binary from my u-boot-spl.bin? I noticed that if I specify zynqmp instead of zynq for -arch, the file size is exactly 256 bytes larger, but it still does not work.
 
Thanks,
 
Gregg
 
  • Sign in to reply
  • Cancel
Parents
  • alamyliu
    0 alamyliu over 8 years ago

    .BIF file

    •   [bootloader] is not U-Boot, it's FSBL
    •   U-Boot is an application to bootgen

     

    BOOT.bif (example)

    image : {

    [bootloader]fsbl/microzed_fsbl.dumpmem.elf

    u-boot.elf

    }

     
    $ bootgen -image boot.bif -o i BOOT.bin
     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • alamyliu
    0 alamyliu over 8 years ago

    .BIF file

    •   [bootloader] is not U-Boot, it's FSBL
    •   U-Boot is an application to bootgen

     

    BOOT.bif (example)

    image : {

    [bootloader]fsbl/microzed_fsbl.dumpmem.elf

    u-boot.elf

    }

     
    $ bootgen -image boot.bif -o i BOOT.bin