Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Problem Booting from SD Card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 373 subscribers
  • Views 533 views
  • Users 0 members are here
Related

Problem Booting from SD Card

e14 Contributor
e14 Contributor over 12 years ago

I am running ISE 14.4. I have created a couple of simple projects that I can run successfully from SDK on the ZED board. One of the projects, for example, is from Xilinx application note UG873(v14.4) - Concepts, Tools, and Techniques. This project is the "Embedded System Design Using PS and PL" in chapter 3. The design uses AXI GPIO and AXI Timer with interrupt.

I am now trying to run the project from the SD card. I built the first stage boot loader and the boot image for the SD card successfully. I copied the boot image, BOOT.BIN, to the SD card so that BOOT.BIN is the only file on the SD card, reconfigured the ZED jumpers for SD booting, and attempted to boot from the SD card. But nothing happens. I don't see the blue LED light when the FPGA is programmed successfully. I know the SD card works because I can reinstall the original boot files for Linux and boot successfully.

I also tried booting the other project that I created, from the SD card, but get the same result.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello Bryan,
    I am not sure how to target my application to run on DDR or OCM. I created my first project by following the example in application note UG873 chapter 3 as I described earlier. I am able to run the application successfully from SDK. The bitstream created successfully. I then created the fsbl and the boot image and programmed the SD card. I followed the procedure given for this in the Zynq introductory Avnet/Speedway seminar book, lab 8 which I attended.

    If there was a choice to choose DDR or OCM to run the application, I don't remember it. Is this referenced in one of the app notes?

    Thanks,

    Bob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello Bryan,
    I am not sure how to target my application to run on DDR or OCM. I created my first project by following the example in application note UG873 chapter 3 as I described earlier. I am able to run the application successfully from SDK. The bitstream created successfully. I then created the fsbl and the boot image and programmed the SD card. I followed the procedure given for this in the Zynq introductory Avnet/Speedway seminar book, lab 8 which I attended.

    If there was a choice to choose DDR or OCM to run the application, I don't remember it. Is this referenced in one of the app notes?

    Thanks,

    Bob